CurveFeatureChainRule Class¶
-
class
NXOpen.
CurveFeatureChainRule
¶ Bases:
NXOpen.SelectionIntentRule
Represents a
NXOpen.SelectionIntentRule
that collects end-to-end connected curves from the feature of the seed.New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
Type | Returns the get the type of selection intent rule: NXOpen.SelectionIntentRule |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetData | Gets the data for the curve feature chain rule: NXOpen.CurveFeatureChainRule |
Method Detail¶
Dispose¶
-
CurveFeatureChainRule.
Dispose
¶ Frees the object from memory.
Signature
Dispose()
New in version NX3.0.0.
License requirements: None.
GetData¶
-
CurveFeatureChainRule.
GetData
¶ Gets the data for the curve feature chain rule:
NXOpen.CurveFeatureChainRule
Signature
GetData()
Returns: a tuple Return type: A tuple consisting of (features, seedCurve, endCurve, fromSeedStart, gapTolerance) features is a list of
NXOpen.Features.Feature
. Features whose curves are used to create this rule seedCurve is aNXOpen.Curve
. Seed curve endCurve is aNXOpen.Curve
. End Curve. It can be null (Nothing)fromSeedStart is a bool. True: the chain starts from the start point of the seed curve gapTolerance is a float. Gap tolerance .. versionadded:: NX3.0.0License requirements: gateway (“UG GATEWAY”)