WedmPointDefinitionBuilder Class¶
-
class
NXOpen.CAM.
WedmPointDefinitionBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAM.WedmPointDefinitionBuilder
This builder cannot be instantiated separately.
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Axis | Returns or sets the wire axis |
AxisOption | Returns or sets the wire axis status |
Point | Returns or sets the wedm point |
PointOption | Returns or sets the point status |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
WedmPointDefinitionBuilderPointStates Enumeration | the types available for wedm point definition |
WedmPointDefinitionBuilderWireAxisStates Enumeration | the types available for wire axis definition |
Property Detail¶
Axis¶
-
WedmPointDefinitionBuilder.
Axis
¶ Returns or sets the wire axis
-------------------------------------
Getter Method
Signature
Axis
Returns: Return type: NXOpen.NXObject
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
Axis
Parameters: newValue ( NXOpen.NXObject
) –New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
AxisOption¶
-
WedmPointDefinitionBuilder.
AxisOption
¶ Returns or sets the wire axis status
-------------------------------------
Getter Method
Signature
AxisOption
Returns: Return type: NXOpen.CAM.WedmPointDefinitionBuilderWireAxisStates
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
AxisOption
Parameters: newValue ( NXOpen.CAM.WedmPointDefinitionBuilderWireAxisStates
) –New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
Point¶
-
WedmPointDefinitionBuilder.
Point
¶ Returns or sets the wedm point
-------------------------------------
Getter Method
Signature
Point
Returns: Return type: NXOpen.Point
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
Point
Parameters: newValue ( NXOpen.Point
) –New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
PointOption¶
-
WedmPointDefinitionBuilder.
PointOption
¶ Returns or sets the point status
-------------------------------------
Getter Method
Signature
PointOption
Returns: Return type: NXOpen.CAM.WedmPointDefinitionBuilderPointStates
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
PointOption
Parameters: newValue ( NXOpen.CAM.WedmPointDefinitionBuilderPointStates
) –New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
WedmPointDefinitionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.