ToolPathTiltMachine Class¶
-
class
NXOpen.CAM.
ToolPathTiltMachine
¶ Bases:
NXOpen.Builder
Represents a Tool Path Tilt Machine Builder
This is a sub-builder class and cannot be directly instantiated
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
MachineMaxStep | Returns the max step distance |
MachineToolMainMcs | Returns or sets the main tool rotation MCS |
MaxTiltAngle | Returns or sets the maximum tilt angle |
MaxToolAxisChange | Returns or sets the tool axis change |
MinTiltAngle | Returns or sets the minimum tilt angle |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ToolPathTiltMachineToolMainMcsTypes Enumeration | the main tool rotation MCS options |
Property Detail¶
MachineMaxStep¶
-
ToolPathTiltMachine.
MachineMaxStep
¶ Returns the max step distance
-------------------------------------
Getter Method
Signature
MachineMaxStep
Returns: the max step distance Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX9.0.0.
License requirements: None.
MachineToolMainMcs¶
-
ToolPathTiltMachine.
MachineToolMainMcs
¶ Returns or sets the main tool rotation MCS
-------------------------------------
Getter Method
Signature
MachineToolMainMcs
Returns: the machine tool main mcs Return type: NXOpen.CAM.ToolPathTiltMachineToolMainMcsTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MachineToolMainMcs
Parameters: machineToolMainMcs ( NXOpen.CAM.ToolPathTiltMachineToolMainMcsTypes
) – the machine tool main mcsNew in version NX9.0.0.
License requirements: None.
MaxTiltAngle¶
-
ToolPathTiltMachine.
MaxTiltAngle
¶ Returns or sets the maximum tilt angle
-------------------------------------
Getter Method
Signature
MaxTiltAngle
Returns: the value of maximal tilt angle Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaxTiltAngle
Parameters: maxTiltangle (float) – the value of maximal tilt angle New in version NX9.0.0.
License requirements: None.
MaxToolAxisChange¶
-
ToolPathTiltMachine.
MaxToolAxisChange
¶ Returns or sets the tool axis change
-------------------------------------
Getter Method
Signature
MaxToolAxisChange
Returns: the value of toolaxis change Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaxToolAxisChange
Parameters: toolaxisChange (float) – the value of maximum tool axis change New in version NX9.0.0.
License requirements: None.
MinTiltAngle¶
-
ToolPathTiltMachine.
MinTiltAngle
¶ Returns or sets the minimum tilt angle
-------------------------------------
Getter Method
Signature
MinTiltAngle
Returns: the value of minimum tilt angle Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MinTiltAngle
Parameters: minTiltangle (float) – the value of minimum tilt angle New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
ToolPathTiltMachine.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.