ToolPathTiltClearance Class¶
-
class
NXOpen.CAM.
ToolPathTiltClearance
¶ Bases:
NXOpen.Builder
Represents a Tool Path Tilt Clearance Builder
This is a sub-builder class and cannot be directly instantiated
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
MinHolderClearance | Returns the minimum holder clearance |
MinNeckClearance | Returns the minimum neck clearance |
MinShankClearance | Returns the minimum shank clearance |
Tag | Returns the Tag for this object. |
TiltClearanceAngle | Returns or sets the tilt clearance angle |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
MinHolderClearance¶
-
ToolPathTiltClearance.
MinHolderClearance
¶ Returns the minimum holder clearance
-------------------------------------
Getter Method
Signature
MinHolderClearance
Returns: the minimum holder clearance value Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX9.0.0.
License requirements: None.
MinNeckClearance¶
-
ToolPathTiltClearance.
MinNeckClearance
¶ Returns the minimum neck clearance
-------------------------------------
Getter Method
Signature
MinNeckClearance
Returns: the minimum neck clearance value Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX9.0.0.
License requirements: None.
MinShankClearance¶
-
ToolPathTiltClearance.
MinShankClearance
¶ Returns the minimum shank clearance
-------------------------------------
Getter Method
Signature
MinShankClearance
Returns: the minimum shank clearance value Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX9.0.0.
License requirements: None.
TiltClearanceAngle¶
-
ToolPathTiltClearance.
TiltClearanceAngle
¶ Returns or sets the tilt clearance angle
-------------------------------------
Getter Method
Signature
TiltClearanceAngle
Returns: the value of tilt clearance angle Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TiltClearanceAngle
Parameters: clearanceValue (float) – the value of tilt clearance angle New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
ToolPathTiltClearance.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.