ToolAxisFixed Class¶
-
class
NXOpen.CAM.
ToolAxisFixed
¶ Bases:
NXOpen.CAM.ToolAxisBase
Represents a Tool Axis Fixed Builder
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
IsPreferredAnglesDefined | Returns the indicator if the preferred angles are defined |
Point | Returns or sets the Point |
PreferredFifthAngle | Returns the preferred fifth angle |
PreferredFourthAngle | Returns the preferred fouth angle |
Tag | Returns the Tag for this object. |
ToolAxisType | Returns or sets the tool axis types |
Vector | Returns or sets the Vector |
Methods¶
Enumerations¶
ToolAxisFixedTypes Enumeration | Available types for Tool Axis Fixed |
Property Detail¶
IsPreferredAnglesDefined¶
-
ToolAxisFixed.
IsPreferredAnglesDefined
¶ Returns the indicator if the preferred angles are defined
-------------------------------------
Getter Method
Signature
IsPreferredAnglesDefined
Returns: the indicator if the preferred angles are defined Return type: bool New in version NX11.0.0.
License requirements: None.
PreferredFifthAngle¶
-
ToolAxisFixed.
PreferredFifthAngle
¶ Returns the preferred fifth angle
-------------------------------------
Getter Method
Signature
PreferredFifthAngle
Returns: the preferred fifth angle Return type: float New in version NX11.0.0.
License requirements: None.
PreferredFourthAngle¶
-
ToolAxisFixed.
PreferredFourthAngle
¶ Returns the preferred fouth angle
-------------------------------------
Getter Method
Signature
PreferredFourthAngle
Returns: the preferred fourth angle Return type: float New in version NX11.0.0.
License requirements: None.
ToolAxisType¶
-
ToolAxisFixed.
ToolAxisType
¶ Returns or sets the tool axis types
-------------------------------------
Getter Method
Signature
ToolAxisType
Returns: the tool axis type Return type: NXOpen.CAM.ToolAxisFixedTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolAxisType
Parameters: toolAxis ( NXOpen.CAM.ToolAxisFixedTypes
) – the tool axis typeNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)