ToolAxisBase Class¶
-
class
NXOpen.CAM.
ToolAxisBase
¶ Bases:
NXOpen.TaggedObject
Represents a tool axis ci Builder
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Point | Returns or sets the Point |
Tag | Returns the Tag for this object. |
Vector | Returns or sets the Vector |
Methods¶
Property Detail¶
Point¶
-
ToolAxisBase.
Point
¶ Returns or sets the Point
-------------------------------------
Getter Method
Signature
Point
Returns: the Point Return type: NXOpen.Point
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Point
Parameters: pointTag ( NXOpen.Point
) – the PointNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
Vector¶
-
ToolAxisBase.
Vector
¶ Returns or sets the Vector
-------------------------------------
Getter Method
Signature
Vector
Returns: the Vector Return type: NXOpen.Direction
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Vector
Parameters: vector ( NXOpen.Direction
) – the VectorNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)