TabPointDataBuilder Class¶
-
class
NXOpen.CAM.
TabPointDataBuilder
¶ Bases:
NXOpen.NXObject
Represents a Tab Point Builder
To create a new instance of this class, use
NXOpen.CAM.WedmCustomBoundaryDataBuilder.CreateTabPointDataBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
EndPoint | Returns or sets the tab end point |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
StartPoint | Returns or sets the tab start point |
TabMethod | Returns or sets the tab method option |
TabThreadMethod | Returns or sets the tab thread method option |
TabThreadPoint | Returns or sets the tab thread point |
TabWidth | Returns or sets the tab Width |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CreateAttributeIterator | Create an attribute iterator |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Enumerations¶
TabPointDataBuilderTabMethodType Enumeration | Tab Point Method Options |
TabPointDataBuilderTabThreadMethodType Enumeration | Tab Thread Point Options |
Property Detail¶
EndPoint¶
-
TabPointDataBuilder.
EndPoint
¶ Returns or sets the tab end point
-------------------------------------
Getter Method
Signature
EndPoint
Returns: the tab end point Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
EndPoint
Parameters: endPoint ( NXOpen.Point
) – the new end point valueNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
IsOccurrence¶
-
TabPointDataBuilder.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
TabPointDataBuilder.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
TabPointDataBuilder.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
TabPointDataBuilder.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
TabPointDataBuilder.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
TabPointDataBuilder.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
StartPoint¶
-
TabPointDataBuilder.
StartPoint
¶ Returns or sets the tab start point
-------------------------------------
Getter Method
Signature
StartPoint
Returns: the tab start point Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
StartPoint
Parameters: startPoint ( NXOpen.Point
) – the new start point valueNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
TabMethod¶
-
TabPointDataBuilder.
TabMethod
¶ Returns or sets the tab method option
-------------------------------------
Getter Method
Signature
TabMethod
Returns: the current tab method Return type: NXOpen.CAM.TabPointDataBuilderTabMethodType
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
TabMethod
Parameters: method ( NXOpen.CAM.TabPointDataBuilderTabMethodType
) – the new tab method valueNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
TabThreadMethod¶
-
TabPointDataBuilder.
TabThreadMethod
¶ Returns or sets the tab thread method option
-------------------------------------
Getter Method
Signature
TabThreadMethod
Returns: the current tab thread method Return type: NXOpen.CAM.TabPointDataBuilderTabThreadMethodType
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
TabThreadMethod
Parameters: threadMethod ( NXOpen.CAM.TabPointDataBuilderTabThreadMethodType
) – the new thread method valueNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
TabThreadPoint¶
-
TabPointDataBuilder.
TabThreadPoint
¶ Returns or sets the tab thread point
-------------------------------------
Getter Method
Signature
TabThreadPoint
Returns: the tab thread point Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
TabThreadPoint
Parameters: threadPoint ( NXOpen.Point
) – the new point valueNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
TabWidth¶
-
TabPointDataBuilder.
TabWidth
¶ Returns or sets the tab Width
-------------------------------------
Getter Method
Signature
TabWidth
Returns: the tab width Return type: float New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
TabWidth
Parameters: tabWidth (float) – the tab width New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
FindObject¶
-
TabPointDataBuilder.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Print¶
-
TabPointDataBuilder.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
TabPointDataBuilder.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.