NcmTurnRoughFinishBuilder Class¶
-
class
NXOpen.CAM.
NcmTurnRoughFinishBuilder
¶ Bases:
NXOpen.CAM.NcmTurningBuilder
Represents a CAM.
NcmTurnRoughFinishBuilder .. versionadded:: NX6.0.0
Properties¶
Property | Description |
---|---|
AvoidanceAfterLastRetract | Returns or sets the prefer direct motion after last retract |
AvoidanceApproachBuilder | Returns the approach path builder |
AvoidanceBetweenRegions | Returns or sets the prefer direct motion between regions |
AvoidanceClearanceBuilder | Returns the clearance builder |
AvoidanceDepartureBuilder | Returns the departure path builder |
AvoidanceForAutomaticEngage | Returns or sets the additional checking for automatic engage |
AvoidanceForAutomaticRetract | Returns or sets the additional checking for automatic retract |
AvoidanceForMinimumClearance | Returns or sets the additional checking for minimum clearance |
AvoidanceFromBuilder | Returns the avoidance from builder |
AvoidanceGohomeBuilder | Returns the gohome point builder |
AvoidanceReturnBuilder | Returns the return path builder |
AvoidanceStartBuilder | Returns the avoidance start builder |
AvoidanceStartOfEngageBuilder | Returns the start of engage builder |
AvoidanceToStartOfEngage | Returns or sets the prefer direct motion to start of engage |
AxialSafeClearance | Returns or sets the axial safe clearance value |
Cutcom | Returns the cutter compensation builder |
DefaultRegionStartType | Returns or sets the region start type |
EngageProfileBuilder | Returns the Profiling Engage builder |
LocalReturnBuilder | Returns the Local Return builder |
NcmHoleMachiningBuilder | Returns the non cutting moves hole machining builder |
RadialSafeClearance | Returns or sets the radial safe clearance value |
RetractProfileBuilder | Returns the Profiling Retract builder |
StartPointsEffectDistBuilder | Returns the region start points effective distance builder (inheritable tool dep) |
StartPointsUseEffectDist | Returns or sets the start points use effective distance |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetCustomizableItemBuilder | Returns the customizable item builder for given customizable item name |
GetCustomizableItemNames | Returns the names for all customizable item ids |
GetRegionStartPoints | Returns region start points |
SetRegionStartPoints | Sets region start points |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AvoidanceForAutomaticEngage¶
-
NcmTurnRoughFinishBuilder.
AvoidanceForAutomaticEngage
¶ Returns or sets the additional checking for automatic engage
-------------------------------------
Getter Method
Signature
AvoidanceForAutomaticEngage
Returns: the additional checking for automatic engage Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AvoidanceForAutomaticEngage
Parameters: avoidanceAutomaticEngage (bool) – the additional checking for automatic engage New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
AvoidanceForAutomaticRetract¶
-
NcmTurnRoughFinishBuilder.
AvoidanceForAutomaticRetract
¶ Returns or sets the additional checking for automatic retract
-------------------------------------
Getter Method
Signature
AvoidanceForAutomaticRetract
Returns: the additional checking for automatic retract Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AvoidanceForAutomaticRetract
Parameters: avoidanceAutomaticRetract (bool) – the additional checking for automatic retract New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
AvoidanceForMinimumClearance¶
-
NcmTurnRoughFinishBuilder.
AvoidanceForMinimumClearance
¶ Returns or sets the additional checking for minimum clearance
-------------------------------------
Getter Method
Signature
AvoidanceForMinimumClearance
Returns: the additional checking for minimum clearance Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AvoidanceForMinimumClearance
Parameters: avoidanceMinimumClearance (bool) – the additional checking for minimum clearance New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
AxialSafeClearance¶
-
NcmTurnRoughFinishBuilder.
AxialSafeClearance
¶ Returns or sets the axial safe clearance value
-------------------------------------
Getter Method
Signature
AxialSafeClearance
Returns: the axial safe clearance value Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AxialSafeClearance
Parameters: axialSafeClearanceValue (float) – the axial safe clearance value New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
EngageProfileBuilder¶
-
NcmTurnRoughFinishBuilder.
EngageProfileBuilder
¶ Returns the Profiling Engage builder
-------------------------------------
Getter Method
Signature
EngageProfileBuilder
Returns: the Profiling Engage builder Return type: NXOpen.CAM.TurnEngageRetractBuilder
New in version NX6.0.0.
License requirements: None.
LocalReturnBuilder¶
-
NcmTurnRoughFinishBuilder.
LocalReturnBuilder
¶ Returns the Local Return builder
-------------------------------------
Getter Method
Signature
LocalReturnBuilder
Returns: the Local Return builder Return type: NXOpen.CAM.TurnRoughFinishLocalReturnBuilder
New in version NX6.0.0.
License requirements: None.
RadialSafeClearance¶
-
NcmTurnRoughFinishBuilder.
RadialSafeClearance
¶ Returns or sets the radial safe clearance value
-------------------------------------
Getter Method
Signature
RadialSafeClearance
Returns: the radial safe clearance value Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RadialSafeClearance
Parameters: radialSafeClearanceValue (float) – the radial safe clearance value New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
RetractProfileBuilder¶
-
NcmTurnRoughFinishBuilder.
RetractProfileBuilder
¶ Returns the Profiling Retract builder
-------------------------------------
Getter Method
Signature
RetractProfileBuilder
Returns: the Profiling Retract builder Return type: NXOpen.CAM.TurnEngageRetractBuilder
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
NcmTurnRoughFinishBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.