NcmHoleDrilling Class¶
-
class
NXOpen.CAM.
NcmHoleDrilling
¶ Bases:
NXOpen.CAM.NcmHoleMachining
Represents a
NXOpen.CAM.NcmHoleDrilling
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
CollisionCheck | Returns or sets the collision check activation |
CutcomMinimumAngle | Returns or sets the cutter compensation minimum angle |
CutcomMinimumMove | Returns the cutter compensation minimum move builder (inheritable tool dep) |
CutcomOutputContactPoint | Returns or sets the cutter compensation output contact point status |
CutcomOutputPlane | Returns or sets the cutter compensation output plane status |
CutcomType | Returns or sets the cutter compensation type |
DefaultRegionStartType | Returns or sets the region start type |
Engage | Returns the engage settings |
FinalRetract | Returns the final retract settings |
FinalSafeDistance | Returns the final safe distance builder (inheritable tool dep) |
FinalType | Returns or sets the final type |
InitialEngage | Returns the initial engage settings |
InitialSafeDistance | Returns the initial safe distance builder (inheritable tool dep) |
InitialType | Returns or sets the initial type |
NcmSmoothing | Returns the non cutting smoothing |
NumberOfThreads | Returns or sets the number of threads |
OverlapAngle | Returns or sets the overlap angle |
OverlapDistance | Returns or sets the overlap distance |
OverlapType | Returns or sets the region start type |
RegionStartAngle | Returns or sets the region start angle |
Retract | Returns the retract settings |
StartFromCenter | Returns or sets the start from center |
StartPointsEffectDistBuilder | Returns the region start points effective distance builder (inheritable tool dep) |
StartPointsUseEffectDist | Returns or sets the start points use effective distance |
SuppressCutcom | Returns or sets the suppress cutter compensation |
Tag | Returns the Tag for this object. |
TrackingData | Returns or sets the tracking data (tracking point type) |
TransferAvoidanceFrom | Returns the from point builder |
TransferAvoidanceGohome | Returns the gohome point builder |
TransferAvoidanceReturn | Returns the return point builder |
TransferAvoidanceStart | Returns the start point builder |
TransferBetweenRegions | Returns the transfer between regions |
TransferClearance | Returns the clearance setting |
TransferInitialFinal | Returns the transfer settings for initial and final |
Methods¶
Method | Description |
---|---|
GetCustomizableItemBuilder | Returns the customizable item builder for given customizable item name |
GetCustomizableItemNames | Returns the names for all customizable item ids |
GetRegionStartPoints | Returns region start points |
SetRegionStartPoints | Sets region start points |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
Validate¶
-
NcmHoleDrilling.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.