NCAssistantBuilder Class¶
-
class
NXOpen.CAM.
NCAssistantBuilder
¶ Bases:
NXOpen.Builder
Represents a NCAssistant Builder
To create a new instance of this class, use
NXOpen.CAM.CAMSetup.CreateNCAssistantBuilder()
Default values.
Property Value AnalysisType Levels AngleTolerance 0.01 (millimeters part),0.01 (inches part) DistanceTolerance 0.01 (millimeters part), 0.0004 (inches part) MaximumAngle 90.00 (millimeters part), 90.00 (inches part) MaximumLevel 1000.00 (millimeters part), 50.00 (inches part) MaximumRadius 50.00 (millimeters part), 2.00 (inches part) MinimumAngle -90.00 (millimeters part), -90.00 (inches part) MinimumLevel -1000.00 (millimeters part), -50.00 (inches part) MinimumRadius -50.00 (millimeters part), -2.00 (inches part) RadiusTolerance 0.01 (millimeters part), 0.0004 (inches part) New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AnalysisType | Returns or sets the Analysis Type |
AngleTolerance | Returns or sets the Angle Tolerance |
DistanceTolerance | Returns or sets the Distance Tolerance |
FacesToAnalyze | Returns the Faces to Analyze |
MaximumAngle | Returns or sets the Maximum Angle |
MaximumLevel | Returns or sets the Maximum Level |
MaximumRadius | Returns or sets the Maximum Radius |
MinimumAngle | Returns or sets the Minimum Angle |
MinimumLevel | Returns or sets the Minimum Level |
MinimumRadius | Returns or sets the Minimum Radius |
RadiusTolerance | Returns or sets the Radius Tolerance |
ReferencePlane | Returns or sets the Reference Plane |
ReferenceVector | Returns or sets the Reference Vector |
SaveFaceColors | Returns or sets the Save Face Colors on Exit |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AnalyzeGeometry | The action of Analyze Geometry button. |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetResults | The analyze result. |
Information | The action of Information button. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
NCAssistantBuilderAnalysisTypes Enumeration | Analysis Type |
Property Detail¶
AnalysisType¶
-
NCAssistantBuilder.
AnalysisType
¶ Returns or sets the Analysis Type
-------------------------------------
Getter Method
Signature
AnalysisType
Returns: the Analysis Type Return type: NXOpen.CAM.NCAssistantBuilderAnalysisTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AnalysisType
Parameters: analysisType ( NXOpen.CAM.NCAssistantBuilderAnalysisTypes
) – the Analysis TypeNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
AngleTolerance¶
-
NCAssistantBuilder.
AngleTolerance
¶ Returns or sets the Angle Tolerance
-------------------------------------
Getter Method
Signature
AngleTolerance
Returns: the Angle Tolerance Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleTolerance
Parameters: angleTolerance (float) – the Angle Tolerance New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
DistanceTolerance¶
-
NCAssistantBuilder.
DistanceTolerance
¶ Returns or sets the Distance Tolerance
-------------------------------------
Getter Method
Signature
DistanceTolerance
Returns: the Distance Tolerance Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance
Parameters: distanceTolerance (float) – the Distance Tolerance New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
FacesToAnalyze¶
-
NCAssistantBuilder.
FacesToAnalyze
¶ Returns the Faces to Analyze
-------------------------------------
Getter Method
Signature
FacesToAnalyze
Returns: the Faces to Analyze Return type: NXOpen.SelectFaceList
New in version NX7.5.0.
License requirements: None.
MaximumAngle¶
-
NCAssistantBuilder.
MaximumAngle
¶ Returns or sets the Maximum Angle
-------------------------------------
Getter Method
Signature
MaximumAngle
Returns: the Maximum Angle Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaximumAngle
Parameters: maximum (float) – the Maximum Angle New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
MaximumLevel¶
-
NCAssistantBuilder.
MaximumLevel
¶ Returns or sets the Maximum Level
-------------------------------------
Getter Method
Signature
MaximumLevel
Returns: the Maximum Level Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaximumLevel
Parameters: maximum (float) – the Maximum Level New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
MaximumRadius¶
-
NCAssistantBuilder.
MaximumRadius
¶ Returns or sets the Maximum Radius
-------------------------------------
Getter Method
Signature
MaximumRadius
Returns: the Maximum Radius Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaximumRadius
Parameters: maximum (float) – the Maximum Radius New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
MinimumAngle¶
-
NCAssistantBuilder.
MinimumAngle
¶ Returns or sets the Minimum Angle
-------------------------------------
Getter Method
Signature
MinimumAngle
Returns: the Minimum Angle Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MinimumAngle
Parameters: minimum (float) – the Minimum Angle New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
MinimumLevel¶
-
NCAssistantBuilder.
MinimumLevel
¶ Returns or sets the Minimum Level
-------------------------------------
Getter Method
Signature
MinimumLevel
Returns: the Minimum Level Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MinimumLevel
Parameters: minimum (float) – the Minimum Level New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
MinimumRadius¶
-
NCAssistantBuilder.
MinimumRadius
¶ Returns or sets the Minimum Radius
-------------------------------------
Getter Method
Signature
MinimumRadius
Returns: the Minimum Radius Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MinimumRadius
Parameters: minimum (float) – the Minimum Radius New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
RadiusTolerance¶
-
NCAssistantBuilder.
RadiusTolerance
¶ Returns or sets the Radius Tolerance
-------------------------------------
Getter Method
Signature
RadiusTolerance
Returns: the Radius Tolerance Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RadiusTolerance
Parameters: radiusTolerance (float) – the Radius Tolerance New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
ReferencePlane¶
-
NCAssistantBuilder.
ReferencePlane
¶ Returns or sets the Reference Plane
-------------------------------------
Getter Method
Signature
ReferencePlane
Returns: the Reference Plane Return type: NXOpen.Plane
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferencePlane
Parameters: referencePlane ( NXOpen.Plane
) – the Reference PlaneNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
ReferenceVector¶
-
NCAssistantBuilder.
ReferenceVector
¶ Returns or sets the Reference Vector
-------------------------------------
Getter Method
Signature
ReferenceVector
Returns: the Reference Vector Return type: NXOpen.Direction
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceVector
Parameters: referenceVector ( NXOpen.Direction
) – the Reference VectorNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
SaveFaceColors¶
-
NCAssistantBuilder.
SaveFaceColors
¶ Returns or sets the Save Face Colors on Exit
-------------------------------------
Getter Method
Signature
SaveFaceColors
Returns: the Save Face Colors on Exit Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SaveFaceColors
Parameters: saveFaceColorsOnExit (bool) – the Save Face Colors on Exit New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
AnalyzeGeometry¶
-
NCAssistantBuilder.
AnalyzeGeometry
¶ The action of Analyze Geometry button.
Signature
AnalyzeGeometry()
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
GetResults¶
-
NCAssistantBuilder.
GetResults
¶ The analyze result.
After analyzing the selected faces,it will return the analyzed faces and the corresponding double values,including depth, corner or fillets radius or draft angle.
Signature
GetResults()
Returns: a tuple Return type: A tuple consisting of (success, analyzedFaces, doubleValue). success is a bool. success or notanalyzedFaces is a list of NXOpen.Face
. the faces found during analyze run, it is need SM_freedoubleValue is a list of float. the corresponding analysis value of the face, depth, corner or fillets radius or draft angleNew in version NX7.5.0.
License requirements: None.
Information¶
-
NCAssistantBuilder.
Information
¶ The action of Information button.
It will bring out a text dialog
Signature
Information()
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
Validate¶
-
NCAssistantBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.