MachiningFeature Class¶
-
class
NXOpen.CAM.
MachiningFeature
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.CAM.CAMFeature
builderTo obtain an instance of this class use
NXOpen.CAM.FeatureRecognitionBuilder
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
CoordinateSystem | Returns or sets the csys feature |
Faces | Returns the face selection |
FeatureType | Returns or sets the feature type of the feature to create |
Features | Returns the list features |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
CoordinateSystem¶
-
MachiningFeature.
CoordinateSystem
¶ Returns or sets the csys feature
-------------------------------------
Getter Method
Signature
CoordinateSystem
Returns: Return type: NXOpen.CoordinateSystem
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CoordinateSystem
Parameters: csysFeature ( NXOpen.CoordinateSystem
) –New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
Faces¶
-
MachiningFeature.
Faces
¶ Returns the face selection
-------------------------------------
Getter Method
Signature
Faces
Returns: Return type: NXOpen.ScCollector
New in version NX8.0.0.
License requirements: None.
FeatureType¶
-
MachiningFeature.
FeatureType
¶ Returns or sets the feature type of the feature to create
-------------------------------------
Getter Method
Signature
FeatureType
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FeatureType
Parameters: name (str) – New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
Features¶
-
MachiningFeature.
Features
¶ Returns the list features
-------------------------------------
Getter Method
Signature
Features
Returns: Return type: NXOpen.CAM.CAMFeatureList
New in version NX8.0.0.
License requirements: None.