LaserTool Class¶
-
class
NXOpen.CAM.
LaserTool
¶ Bases:
NXOpen.CAM.SoftTool
Represents a Laser Tool
To create a new instance of this class, use
NXOpen.CAM.NCGroupCollection.CreateLaserTool()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
ChannelName | Returns or sets the channel’s name |
CutterExportBuilder | Returns the cutter export builder |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
Diameter | Returns the Nozzle Diameter |
EndUdeSet | Returns the end ude set |
FocalDiameter | Returns the Focal Diameter |
FocalDistance | Returns the Focal Distance |
HolderDescription | Returns or sets the holder description |
HolderLibraryReference | Returns or sets the holder libref |
HolderSection | Returns the holder sections |
Length | Returns the Nozzle Length |
LibraryParametersBuilder | Returns the Library Data Object |
MaxPower | Returns the Maximum Power |
MinPower | Returns the Minimum Power |
OptimizationMethod | Returns or sets the optim method |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
TaperLength | Returns the Nozzle Taper Length |
TipDiameter | Returns the Nozzle Tip Diameter |
TlCtlgNum | Returns or sets the Catalog Number |
TlDescription | Returns or sets the Cutter Description |
TlHolderNumberBuilder | Returns the Holder Number |
TlLibref | Returns or sets the Cutter Libref |
TlManualToolChange | Returns or sets the Manual Tool Change |
TlNumberBuilder | Returns the Tool Number |
TlText | Returns or sets the tool text |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCustomizableItemBuilder | Returns the customizable item builder for the given customizable item name |
GetCustomizableItemNames | Returns the names for all customizable item ids |
GetMaterial | Get tool material |
GetMaterialData | Get material data |
GetObject | Returns the object currently being edited by this builder. |
SetMaterial | Set tool material |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Diameter¶
-
LaserTool.
Diameter
¶ Returns the Nozzle Diameter
-------------------------------------
Getter Method
Signature
Diameter
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX9.0.0.
License requirements: None.
FocalDiameter¶
-
LaserTool.
FocalDiameter
¶ Returns the Focal Diameter
-------------------------------------
Getter Method
Signature
FocalDiameter
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX9.0.0.
License requirements: None.
FocalDistance¶
-
LaserTool.
FocalDistance
¶ Returns the Focal Distance
-------------------------------------
Getter Method
Signature
FocalDistance
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX9.0.0.
License requirements: None.
Length¶
-
LaserTool.
Length
¶ Returns the Nozzle Length
-------------------------------------
Getter Method
Signature
Length
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX9.0.0.
License requirements: None.
MaxPower¶
-
LaserTool.
MaxPower
¶ Returns the Maximum Power
-------------------------------------
Getter Method
Signature
MaxPower
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX9.0.0.
License requirements: None.
MinPower¶
-
LaserTool.
MinPower
¶ Returns the Minimum Power
-------------------------------------
Getter Method
Signature
MinPower
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX9.0.0.
License requirements: None.
TaperLength¶
-
LaserTool.
TaperLength
¶ Returns the Nozzle Taper Length
-------------------------------------
Getter Method
Signature
TaperLength
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX9.0.0.
License requirements: None.
TipDiameter¶
-
LaserTool.
TipDiameter
¶ Returns the Nozzle Tip Diameter
-------------------------------------
Getter Method
Signature
TipDiameter
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
LaserTool.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.