InterpolateAngle Class¶
-
class
NXOpen.CAM.
InterpolateAngle
¶ Bases:
NXOpen.CAM.ToolAxisInterpolate
Represents builder of Interpolate Angle, one option of Tool Axis
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
ControlDirection | Returns or sets the control direction type |
InterpolationMethod | Returns or sets the interpolation method type |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Erase | Delete an existing item by index |
GetLeadAngle | Get the lead angle |
GetPoint | Get the point |
GetTiltAngle | Get the tilt angle |
GetTotalNumberOfPoints | Get the total number of interpolate data points |
Insert | Add a new item |
Modify | Modify an existing item by index |
MoveDown | Move down an item |
MoveUp | Move up an item |
ResetToDefault | The action of Reset to Default |
Method Detail¶
Erase¶
-
InterpolateAngle.
Erase
¶ Delete an existing item by index
Signature
Erase(index)
Parameters: index (int) – the index of deleted item New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
GetLeadAngle¶
-
InterpolateAngle.
GetLeadAngle
¶ Get the lead angle
Signature
GetLeadAngle(index)
Parameters: index (int) – the index of item Returns: the lead angle Return type: float New in version NX7.5.5.
License requirements: None.
GetTiltAngle¶
-
InterpolateAngle.
GetTiltAngle
¶ Get the tilt angle
Signature
GetTiltAngle(index)
Parameters: index (int) – the index of item Returns: the tilt angle Return type: float New in version NX7.5.5.
License requirements: None.
Insert¶
-
InterpolateAngle.
Insert
¶ Add a new item
Signature
Insert(inputIndex, point, view, leadAngle, tiltAngle)
Parameters: - inputIndex (int) – the new created item index
- point (
NXOpen.Point
) – the point - view (
NXOpen.NXObject
) – the view - leadAngle (float) – the lead angle
- tiltAngle (float) – the tilt angle
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
Modify¶
-
InterpolateAngle.
Modify
¶ Overloaded method Modify
Modify(index, point, tiltAngle, leadAngle)
Modify(index, point, tiltAngle, leadAngle, ignorePoint)
-------------------------------------
Modify an existing item by index
Signature
Modify(index, point, tiltAngle, leadAngle)
Parameters: - index (int) – the index of modified item
- point (
NXOpen.Point
) – the point - tiltAngle (float) – the tilt angle
- leadAngle (float) – the lead angle
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Modify an existing item by index
Signature
Modify(index, point, tiltAngle, leadAngle, ignorePoint)
Parameters: - index (int) – the index of modified item
- point (
NXOpen.Point
) – the point - tiltAngle (float) – the tilt angle
- leadAngle (float) – the lead angle
- ignorePoint (bool) – the ignore point status
New in version NX11.0.2.
License requirements: cam_base (“CAM BASE”)
-------------------------------------