InspectionPointFeatureBuilder Class¶
-
class
NXOpen.CAM.
InspectionPointFeatureBuilder
¶ Bases:
NXOpen.CAM.OperationBuilder
Represents a CMM Inspection Point Feature builder
To create a new instance of this class, use
NXOpen.CAM.InspectionOperationCollection.CreateInspectionPointFeatureBuilder()
New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
ChannelName | Returns or sets the channel’s name |
CsysReferenceType | Returns or sets the coordinate system reference type |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndOfPath | Returns the end event builder |
EndUdeSet | Returns the end ude set |
Geometry | Returns the geometry builder |
GougeChecking | Returns or sets the gouge checking flag |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
LayoutAndLayer | Returns the Layer and Layout |
MotionOutputBuilder | Returns the motion output builder |
Name | Returns or sets the name of the inspection point feature |
NormalVectorI | Returns or sets the normal vector I component |
NormalVectorJ | Returns or sets the normal vector J component |
NormalVectorK | Returns or sets the normal vector K component |
Notes | Returns the notes builder |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
PathDisplayOptions | Returns the path display options builder |
PointX | Returns or sets the point X coordinate |
PointY | Returns or sets the point Y coordinate |
PointZ | Returns or sets the point Z coordinate |
PostToolPathExit | Returns or sets the environment variable that points to the post tool path generation library which has the exit |
ProjectToFace | Returns or sets the project point to face option |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
ReverseDirection | Returns or sets the reverse normal vector direction button |
SafeClearance | Returns the safe clearance builder |
SelectPoint | Returns or sets the selected point |
SelectProjectionFaces | Returns the selected projection faces |
SelectToolFlag | Returns or sets the user selected tool |
StartOfPath | Returns the start event builder |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
ToolChangeSetting | Returns the tool change builder |
ToolPathEditor | Returns the Tool Path Editor Builder |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
FlipNormal | Flips the point inspection feature normal vector |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCustomizableItemBuilder | Returns the customizable item builder for the given customizable item name |
GetCustomizableItemNames | Returns the names for all customizable item ids |
GetHoleAxisValues | Get the Hole Axis values |
GetObject | Returns the object currently being edited by this builder. |
SetHoleAxisValues | Set the Hole Axis values |
SetProjectionFaces | Sets the point inspection feature projection faces |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateParams | Updates point inspection feature characteristic parameters based on selected geometry |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CsysReferenceType¶
-
InspectionPointFeatureBuilder.
CsysReferenceType
¶ Returns or sets the coordinate system reference type
-------------------------------------
Getter Method
Signature
CsysReferenceType
Returns: Return type: NXOpen.CAM.CamInspectionOperationCsysreferencetypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CsysReferenceType
Parameters: csysReferenceType ( NXOpen.CAM.CamInspectionOperationCsysreferencetypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Name¶
-
InspectionPointFeatureBuilder.
Name
¶ Returns or sets the name of the inspection point feature
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name
Parameters: name (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
NormalVectorI¶
-
InspectionPointFeatureBuilder.
NormalVectorI
¶ Returns or sets the normal vector I component
-------------------------------------
Getter Method
Signature
NormalVectorI
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalVectorI
Parameters: normalVectorI (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
NormalVectorJ¶
-
InspectionPointFeatureBuilder.
NormalVectorJ
¶ Returns or sets the normal vector J component
-------------------------------------
Getter Method
Signature
NormalVectorJ
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalVectorJ
Parameters: normalVectorJ (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
NormalVectorK¶
-
InspectionPointFeatureBuilder.
NormalVectorK
¶ Returns or sets the normal vector K component
-------------------------------------
Getter Method
Signature
NormalVectorK
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalVectorK
Parameters: normalVectorK (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PointX¶
-
InspectionPointFeatureBuilder.
PointX
¶ Returns or sets the point X coordinate
-------------------------------------
Getter Method
Signature
PointX
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointX
Parameters: pointX (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PointY¶
-
InspectionPointFeatureBuilder.
PointY
¶ Returns or sets the point Y coordinate
-------------------------------------
Getter Method
Signature
PointY
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointY
Parameters: pointY (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PointZ¶
-
InspectionPointFeatureBuilder.
PointZ
¶ Returns or sets the point Z coordinate
-------------------------------------
Getter Method
Signature
PointZ
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointZ
Parameters: pointZ (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ProjectToFace¶
-
InspectionPointFeatureBuilder.
ProjectToFace
¶ Returns or sets the project point to face option
-------------------------------------
Getter Method
Signature
ProjectToFace
Returns: Return type: bool New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProjectToFace
Parameters: project (bool) – New in version NX11.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ReverseDirection¶
-
InspectionPointFeatureBuilder.
ReverseDirection
¶ Returns or sets the reverse normal vector direction button
-------------------------------------
Getter Method
Signature
ReverseDirection
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseDirection
Parameters: reverseDirection (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SelectPoint¶
-
InspectionPointFeatureBuilder.
SelectPoint
¶ Returns or sets the selected point
-------------------------------------
Getter Method
Signature
SelectPoint
Returns: Return type: NXOpen.Point
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectPoint
Parameters: selectPoint ( NXOpen.Point
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SelectProjectionFaces¶
-
InspectionPointFeatureBuilder.
SelectProjectionFaces
¶ Returns the selected projection faces
-------------------------------------
Getter Method
Signature
SelectProjectionFaces
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX7.0.0.
License requirements: None.
Method Detail¶
FlipNormal¶
-
InspectionPointFeatureBuilder.
FlipNormal
¶ Flips the point inspection feature normal vector
Signature
FlipNormal()
New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SetProjectionFaces¶
-
InspectionPointFeatureBuilder.
SetProjectionFaces
¶ Sets the point inspection feature projection faces
Signature
SetProjectionFaces(projectionFaces)
Parameters: projectionFaces (list of NXOpen.Face
) – Array of projection facesNew in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UpdateParams¶
-
InspectionPointFeatureBuilder.
UpdateParams
¶ Updates point inspection feature characteristic parameters based on selected geometry
Signature
UpdateParams()
New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Validate¶
-
InspectionPointFeatureBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.