GuidingCurvesCutDir Class¶
-
class
NXOpen.CAM.
GuidingCurvesCutDir
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a guiding curves cut dir type
This is an abstract class and cannot be instantiated.
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
CutDir | Returns or sets the guiding curves cut direction used for common block |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
GuidingCurvesCutDirOption Enumeration | Enum of guiding curves cut direction |
Property Detail¶
CutDir¶
-
GuidingCurvesCutDir.
CutDir
¶ Returns or sets the guiding curves cut direction used for common block
-------------------------------------
Getter Method
Signature
CutDir
Returns: the guiding_curves_cut_dir value Return type: NXOpen.CAM.GuidingCurvesCutDirOption
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutDir
Parameters: guidingCurvesCutDir ( NXOpen.CAM.GuidingCurvesCutDirOption
) – the guiding_curves_cut_dir valueNew in version NX12.0.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
GuidingCurvesCutDir.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.