GuidingCurvesCutDirOption Enumeration¶
NXOpen.CAM.GuidingCurvesCutDir.Option is an alias for NXOpen.CAM.GuidingCurvesCutDirOption
-
class
NXOpen.CAM.
GuidingCurvesCutDirOption
¶ Bases:
object
Enum of guiding curves cut direction
Enum Members
Enum Member Enum Member Description Clockwise Cut direction is clockwise Counterclockwise Cut direction is counterclockwise AlongGuide Cut direction is along the guide curve OppositeGuide Cut direction is opposite the guide curve -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-