GenericTrackingBuilder Class

class NXOpen.CAM.GenericTrackingBuilder

Bases: NXOpen.CAM.SolidTrackingBuilder

Represents a GenericTracking Builder

To create a new instance of this class, use NXOpen.CAM.Tool.CreateGenericTrackingBuilder()

New in version NX5.0.0.

Properties

Property Description
Location Returns or sets the location
Tag Returns the Tag for this object.
TlAdjReg Returns or sets the adjust register
TlCutcomReg Returns or sets the cutcom register
TrackingName Returns or sets the Tracking Point name value
TrackingXOff Returns or sets the XOff value
TrackingYOff Returns or sets the YOff value
TrackingZOff Returns or sets the ZOff value

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Method Detail

Validate

GenericTrackingBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.