TrackpointBuilder Class¶
-
class
NXOpen.CAM.
TrackpointBuilder
¶ Bases:
NXOpen.Builder
Represents a Trackpoint Builder
This is an abstract class and can not be instantiated
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
TlAdjReg | Returns or sets the adjust register |
TlCutcomReg | Returns or sets the cutcom register |
TrackingName | Returns or sets the Tracking Point name value |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
TlAdjReg¶
-
TrackpointBuilder.
TlAdjReg
¶ Returns or sets the adjust register
-------------------------------------
Getter Method
Signature
TlAdjReg
Returns: the tool adjust register Return type: int New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
TlAdjReg
Parameters: tlAdjReg (int) – The adjust register New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
TlCutcomReg¶
-
TrackpointBuilder.
TlCutcomReg
¶ Returns or sets the cutcom register
-------------------------------------
Getter Method
Signature
TlCutcomReg
Returns: the tool cutcom register Return type: int New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
TlCutcomReg
Parameters: tlCutcomReg (int) – The cutcom register New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
TrackingName¶
-
TrackpointBuilder.
TrackingName
¶ Returns or sets the Tracking Point name value
-------------------------------------
Getter Method
Signature
TrackingName
Returns: the tracking name value Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TrackingName
Parameters: nameValue (str) – the name value New in version NX5.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
TrackpointBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.