FollowGeometryMoveBuilder Class¶
-
class
NXOpen.CAM.
FollowGeometryMoveBuilder
¶ Bases:
NXOpen.CAM.MoveBuilder
Represents the Follow Geometry Move Builder
This is an abstract class, and cannot be created.
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
EndExtension | Returns or sets the end extension |
FeedRate | Returns or sets the feed rate |
FeedType | Returns or sets the feed type |
FeedUnit | Returns or sets the feed unit |
MotionType | Returns or sets the motion type |
NumberOfUserParameters | Returns the number of user parameters |
ProtectedMove | Returns or sets the protected move status |
StartExtension | Returns or sets the start extension |
StartPoint | Returns or sets the start location |
StartToolAxis | Returns or sets the start tool axis |
SubopLabel | Returns or sets the subop label |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetUserParameter | Returns the custom parameter with the given name. |
SetParent | Set parent |
SetSibling | Set sibling |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
EndExtension¶
-
FollowGeometryMoveBuilder.
EndExtension
¶ Returns or sets the end extension
-------------------------------------
Getter Method
Signature
EndExtension
Returns: Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndExtension
Parameters: builderTag ( NXOpen.CAM.InheritableToolDepBuilder
) –New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
StartExtension¶
-
FollowGeometryMoveBuilder.
StartExtension
¶ Returns or sets the start extension
-------------------------------------
Getter Method
Signature
StartExtension
Returns: Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartExtension
Parameters: builderTag ( NXOpen.CAM.InheritableToolDepBuilder
) –New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
StartPoint¶
-
FollowGeometryMoveBuilder.
StartPoint
¶ Returns or sets the start location
-------------------------------------
Getter Method
Signature
StartPoint
Returns: Return type: NXOpen.Point
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartPoint
Parameters: location ( NXOpen.Point
) –New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
StartToolAxis¶
-
FollowGeometryMoveBuilder.
StartToolAxis
¶ Returns or sets the start tool axis
-------------------------------------
Getter Method
Signature
StartToolAxis
Returns: Return type: NXOpen.Direction
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartToolAxis
Parameters: vec ( NXOpen.Direction
) –New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
FollowGeometryMoveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.