FinishTurningBuilder Class¶
-
class
NXOpen.CAM.
FinishTurningBuilder
¶ Bases:
NXOpen.CAM.RoughFinishTurningBuilder
Represents a FinishTurning Builder
To create a new instance of this class, use
NXOpen.CAM.OperationCollection.CreateFinishTurningBuilder()
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AdditionalCommands | Returns or sets the Additional Commands |
AxialTrimPlane1 | Returns the axial trim plane 1 |
AxialTrimPlane2 | Returns the axial trim plane 2 |
ChannelName | Returns or sets the channel’s name |
CustomMemberData | Returns or sets the Custom Member Data type |
CustomMemberDataDistance | Returns or sets the Custom Member Data Distance |
CustomPartBoundary | Returns the custom part boundary builder |
CutParameters | Returns the cut parameter object |
CutRegions | Returns or sets the Cut regions type |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndAngle | Returns or sets the end angle |
EndOfPath | Returns the end event builder |
EndOffset | Returns or sets the end offset |
EndUdeSet | Returns the end ude set |
ExtendMode | Returns or sets the Extend Mode |
FeedsBuilder | Returns the feeds and speeds builder |
FlipToolAroundHolder | Returns or sets the Flip Tool Around Holder toggle |
Geometry | Returns the geometry builder |
GougeChecking | Returns or sets the gouge checking flag |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
IgnoreMinimumBoringDiameter | Returns or sets the Ignore Minimum Boring Diameter toggle |
LayoutAndLayer | Returns the Layer and Layout |
LevelAngleBuilder | Returns the Level Angle |
MachineCycleSubroutineName | Returns or sets the machine cycle subroutine name |
MaximumAreaMode | Returns or sets the Maximum Area mode |
MaximumAreaSize | Returns or sets the Maximum Area Size |
MaximumAreaUnit | Returns or sets the Maximum Area Unit |
MaximumSizeAxial | Returns the Maximum Size Axial |
MaximumSizeMode | Returns or sets the Maximum Size Mode |
MaximumSizeRadial | Returns the Maximum Size Radial |
MinimumArea | Returns or sets the Minimum Area type |
MinimumAreaSize | Returns or sets the Minimum Area Size |
MinimumAreaUnit | Returns or sets the Minimum Area Unit |
MinimumSizeAxial | Returns the Minimum Size Axial |
MinimumSizeMode | Returns or sets the Minimum Size Mode |
MinimumSizeRadial | Returns the Minimum Size Radial |
MotionOutput | Returns or sets the motion output |
MotionOutputBuilder | Returns the motion output builder |
NonCuttingBuilder | Returns the non-cutting builder |
Notes | Returns the notes builder |
OmitReversals | Returns or sets the Omit Reversals toggle |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
PathDisplayOptions | Returns the path display options builder |
PostToolPathExit | Returns or sets the environment variable that points to the post tool path generation library which has the exit |
RadialTrimPlane1 | Returns the radial trim plane 1 |
RadialTrimPlane2 | Returns the radial trim plane 2 |
RegionMachining | Returns or sets the Region Machining type |
RegionSelection | Returns or sets the Region Selection type |
RegionSelectionPoint | Returns or sets the Region Selection Point |
ReorientToolHolder | Returns or sets the Reorient Tool Holder toggle. |
ReorientToolHolderMode | Returns or sets the Reorient Tool Holder Mode |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
RotateTrackingPoint | Returns or sets the Rotate Tracking Point toggle |
SafeClearance | Returns the safe clearance builder |
SelectToolFlag | Returns or sets the user selected tool |
StartAngle | Returns or sets the start angle |
StartOfPath | Returns the start event builder |
StartOffset | Returns or sets the Start Offset |
StartUdeSet | Returns the start ude set |
StepAngleBuilder | Returns the Step Angle |
Tag | Returns the Tag for this object. |
ToleranceOffset | Returns or sets the Tolerance Offset type |
ToolChangeSetting | Returns the tool change builder |
ToolHolderAngle | Returns the Tool Holder Angle |
ToolPathEditor | Returns the Tool Path Editor Builder |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
TrackingPointStatus | Returns or sets the tracking point status |
TrimPoint1 | Returns the trim point 1 |
TrimPoint2 | Returns the trim point 2 |
UpdateIpw | Returns or sets the update IPW mode |
UseMachineCycle | Returns or sets the Use Machine Cycle toggle |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCustomizableItemBuilder | Returns the customizable item builder for the given customizable item name |
GetCustomizableItemNames | Returns the names for all customizable item ids |
GetHoleAxisValues | Get the Hole Axis values |
GetObject | Returns the object currently being edited by this builder. |
SetHoleAxisValues | Set the Hole Axis values |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
NonCuttingBuilder¶
-
FinishTurningBuilder.
NonCuttingBuilder
¶ Returns the non-cutting builder
-------------------------------------
Getter Method
Signature
NonCuttingBuilder
Returns: the non-cutting builder Return type: NXOpen.CAM.NcmTurnRoughFinishBuilder
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
FinishTurningBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.