DrillSurfaceBuilder Class¶
-
class
NXOpen.CAM.
DrillSurfaceBuilder
¶ Bases:
NXOpen.TaggedObject
Represents a Drill Surface Builder
This is an abstract class and cannot be instantiated.
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Surface | Returns or sets the selected surface,surface entity type covers Xform,Plane and Face |
SurfaceOption | Returns or sets the surface option |
Tag | Returns the Tag for this object. |
ZcConstant | Returns or sets the zc constant, will create one plane based on this value |
Methods¶
Enumerations¶
DrillSurfaceBuilderSurfaceType Enumeration | Drill surface type |
Property Detail¶
Surface¶
-
DrillSurfaceBuilder.
Surface
¶ Returns or sets the selected surface,surface entity type covers Xform,Plane and Face
-------------------------------------
Getter Method
Signature
Surface
Returns: entity type can be XFORM, PLANE or FACE Return type: NXOpen.NXObject
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Surface
Parameters: surface ( NXOpen.NXObject
) – entity type can be XFORM, PLANE or FACE.If surface type is PLANE, zcConstant value also is changed based on itNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
SurfaceOption¶
-
DrillSurfaceBuilder.
SurfaceOption
¶ Returns or sets the surface option
-------------------------------------
Getter Method
Signature
SurfaceOption
Returns: Return type: NXOpen.CAM.DrillSurfaceBuilderSurfaceType
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SurfaceOption
Parameters: surfaceOption ( NXOpen.CAM.DrillSurfaceBuilderSurfaceType
) –New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
ZcConstant¶
-
DrillSurfaceBuilder.
ZcConstant
¶ Returns or sets the zc constant, will create one plane based on this value
-------------------------------------
Getter Method
Signature
ZcConstant
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZcConstant
Parameters: zcConstant (float) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)