DrillBoringBarTool Class¶
-
class
NXOpen.CAM.
DrillBoringBarTool
¶ Bases:
NXOpen.CAM.DrillToolBuilder
Represents a new Boring Bar Tool Builder
To create a new instance of this class, use
NXOpen.CAM.NCGroupCollection.CreateDrillBoringBarTool()
New in version NX11.0.1.
Properties¶
Property | Description |
---|---|
BackInsertLength | Returns the Back Insert Length |
ChannelName | Returns or sets the channel’s name |
CoolantThrough | Returns or sets the coolant through parameter |
CutterExportBuilder | Returns the cutter export builder |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndUdeSet | Returns the end ude set |
FrontInsertLength | Returns the Front Insert Length |
HelicalDiameter | Returns the helical diameter |
HelicalRampAngle | Returns the ramp angle |
HolderDescription | Returns or sets the holder description |
HolderLibraryReference | Returns or sets the holder libref |
HolderSectionBuilder | Returns the holder sections builder |
InsertAngle | Returns the Insert Angle |
LeadAngle | Returns the Lead Angle |
LibraryParametersBuilder | Returns the Library Data Object |
MaxCutWidth | Returns the max cut width |
MillingTrackpointBuilder | Returns the mill trackpoint builder |
MinRampLength | Returns the min ramp length |
OptimizationMethod | Returns or sets the optim method |
ReliefLength | Returns the Relief Length |
ReliefWidth | Returns the Relief Width |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
TaperedShankDiameterBuilder | Returns the tapered shank diameter |
TaperedShankLengthBuilder | Returns the tapered shank length |
TaperedShankTaperLengthBuilder | Returns the tapered shank taper length |
TlAdjRegBuilder | Returns the Adjust Register |
TlCoolantThro | Returns or sets the coolant through |
TlCor1RadBuilder | Returns the Corner Radius builder (inheritable double) |
TlCtlgNum | Returns or sets the Catalog Number |
TlCutcomReg | Returns or sets the Cutcom Register |
TlCutcomRegBuilder | Returns the Cutcom Register Builder |
TlDescription | Returns or sets the Cutter Description |
TlDesignation | Returns or sets the Designation |
TlDiameterBuilder | Returns the Tool Diameter builder (inheritable double) |
TlDirection | Returns or sets the tool direction |
TlFluteLnBuilder | Returns the flute length |
TlHeightBuilder | Returns the length |
TlHolderDescription | Returns or sets the Holder Description |
TlHolderLibref | Returns or sets the Holder Library Reference |
TlHolderNumberBuilder | Returns the Holder Number |
TlIncludedAngBuilder | Returns the Included Angle builder (inheritable double) |
TlLibref | Returns or sets the Cutter Libref |
TlLowCorRadBuilder | Returns the low corner radius |
TlManualToolChange | Returns or sets the Manual Tool Change |
TlNumFlutesBuilder | Returns the Number of Flutes builder (inheritable integer) |
TlNumberBuilder | Returns the Tool Number |
TlPilotDiaBuilder | Returns the pilot diameter builder (inheritable double) |
TlPilotLengthBuilder | Returns the pilot length builder (inheritable double) |
TlPitchBuilder | Returns the Pitch builder (inheritable double) |
TlPointAngBuilder | Returns the Point Angle builder (inheritable double) |
TlPointLengthBuilder | Returns the Point Length builder (inheritable double) |
TlShankDiaBuilder | Returns the Shank Diameter builder (inheritable double) |
TlTaperAngBuilder | Returns the Taper Angle builder (inheritable double) |
TlTaperDiaDistBuilder | Returns the Taper Diameter Distance builder (inheritable double) |
TlText | Returns or sets the tool text |
TlTipDiameterBuilder | Returns the Tip Diameter builder (inheritable double) |
TlTipLengthBuilder | Returns the Tip Length builder (inheritable double) |
TlUpCorRadBuilder | Returns the up corner radius |
TlXOffsetBuilder | Returns the X Offset builder (inheritable double) |
TlYzOffsetBuilder | Returns the YZ Offset builder (inheritable double) |
TlZMountBuilder | Returns the Z Mount builder (inheritable double) |
TlZOffsetBuilder | Returns the Z Offset builder (inheritable double) |
UseTaperedShank | Returns or sets the use tapered shank |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCustomizableItemBuilder | Returns the customizable item builder for the given customizable item name |
GetCustomizableItemNames | Returns the names for all customizable item ids |
GetMaterial | Get tool material |
GetMaterialData | Get material data |
GetObject | Returns the object currently being edited by this builder. |
SetMaterial | Set tool material |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BackInsertLength¶
-
DrillBoringBarTool.
BackInsertLength
¶ Returns the Back Insert Length
-------------------------------------
Getter Method
Signature
BackInsertLength
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX11.0.1.
License requirements: None.
FrontInsertLength¶
-
DrillBoringBarTool.
FrontInsertLength
¶ Returns the Front Insert Length
-------------------------------------
Getter Method
Signature
FrontInsertLength
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX11.0.1.
License requirements: None.
InsertAngle¶
-
DrillBoringBarTool.
InsertAngle
¶ Returns the Insert Angle
-------------------------------------
Getter Method
Signature
InsertAngle
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX11.0.1.
License requirements: None.
LeadAngle¶
-
DrillBoringBarTool.
LeadAngle
¶ Returns the Lead Angle
-------------------------------------
Getter Method
Signature
LeadAngle
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX11.0.1.
License requirements: None.
ReliefLength¶
-
DrillBoringBarTool.
ReliefLength
¶ Returns the Relief Length
-------------------------------------
Getter Method
Signature
ReliefLength
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX11.0.1.
License requirements: None.
ReliefWidth¶
-
DrillBoringBarTool.
ReliefWidth
¶ Returns the Relief Width
-------------------------------------
Getter Method
Signature
ReliefWidth
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX11.0.1.
License requirements: None.
Method Detail¶
Validate¶
-
DrillBoringBarTool.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.