CylindricalMillingCutParameters Class¶
-
class
NXOpen.CAM.
CylindricalMillingCutParameters
¶ Bases:
NXOpen.CAM.FeatureMillingCutParameters
Represents a CylindricalMillingCutParameters Builder
This is an abstract class and cannot be instantiated.
New in version NX9.0.2.
Properties¶
Property | Description |
---|---|
BottomOffset | Returns the bottom offset |
BottomStock | Returns the bottom stock |
CheckIpwCollisions | Returns or sets the value to Check for Ipw Collsions |
CheckSafeClearance | Returns the Check Safe Clearance |
ContinuousCut | Returns or sets the continuous cut |
CornerControl | Returns the corner control |
CuttingDirection | Returns or sets the cut direction |
HolderClearance | Returns the Holder Clearance |
IpwType | Returns or sets the IPW type |
NeckClearance | Returns the Neck Clearance |
PartSafeClearance | Returns the Part Safe Clearance |
PartStock | Returns the part stock |
ShankClearance | Returns the Shank Clearance |
Tag | Returns the Tag for this object. |
Tolerances | Returns the Tolerances builder |
TopOffset | Returns the top offset |
UseToolHolder | Returns or sets the use tool holder |
Methods¶
Property Detail¶
BottomOffset¶
-
CylindricalMillingCutParameters.
BottomOffset
¶ Returns the bottom offset
-------------------------------------
Getter Method
Signature
BottomOffset
Returns: the bottom offset builder Return type: NXOpen.CAM.VerticalPosition
New in version NX9.0.2.
License requirements: None.
ContinuousCut¶
-
CylindricalMillingCutParameters.
ContinuousCut
¶ Returns or sets the continuous cut
-------------------------------------
Getter Method
Signature
ContinuousCut
Returns: the continuous cut Return type: bool New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
ContinuousCut
Parameters: continuousCut (bool) – the continuous cut New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)