HoleMachiningCutParameters Class¶
-
class
NXOpen.CAM.
HoleMachiningCutParameters
¶ Bases:
NXOpen.CAM.CutParameters
Represents a HoleMachiningCutParameters Builder
This is an abstract class and cannot be instantiated.
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
BottomStock | Returns the bottom stock |
CheckIpwCollisions | Returns or sets the value to Check for Ipw Collsions |
CheckSafeClearance | Returns the Check Safe Clearance |
CornerControl | Returns the corner control |
HolderClearance | Returns the Holder Clearance |
IpwType | Returns or sets the IPW type |
NeckClearance | Returns the Neck Clearance |
PartSafeClearance | Returns the Part Safe Clearance |
PartStock | Returns the part stock |
ShankClearance | Returns the Shank Clearance |
Tag | Returns the Tag for this object. |
Tolerances | Returns the Tolerances builder |
TopOffset | Returns the top offset |
UseToolHolder | Returns or sets the use tool holder |
Methods¶
Property Detail¶
BottomStock¶
-
HoleMachiningCutParameters.
BottomStock
¶ Returns the bottom stock
-------------------------------------
Getter Method
Signature
BottomStock
Returns: the bottom stock Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX9.0.2.
License requirements: None.
CornerControl¶
-
HoleMachiningCutParameters.
CornerControl
¶ Returns the corner control
-------------------------------------
Getter Method
Signature
CornerControl
Returns: Return type: NXOpen.CAM.CornerControlBuilder
New in version NX11.0.2.
License requirements: None.
TopOffset¶
-
HoleMachiningCutParameters.
TopOffset
¶ Returns the top offset
-------------------------------------
Getter Method
Signature
TopOffset
Returns: the top offset builder Return type: NXOpen.CAM.VerticalPosition
New in version NX9.0.2.
License requirements: None.