CamOperationMotionContactDataType Struct

class NXOpen.CAM.CamOperationMotionContactDataType

Bases: object

Motion contact data type .

Constructor: NXOpen.CAM.CamOperationMotionContactDataType()

Fields

Field Description
ContactPt If motion is contact, this is the contact position.
ContactArcAxis  
ContactArcCenter Contact arc center
ContactArcRadius Contact arc radius
ContactShape  

ContactPt

CamOperationMotionContactDataType.ContactPt

If motion is contact, this is the contact position.

-------------------------------------

Field Value Type:NXOpen.CAM.CamOperationMotionPosType

ContactArcAxis

CamOperationMotionContactDataType.ContactArcAxis

-------------------------------------

Field Value Type:NXOpen.Vector3d

ContactArcCenter

CamOperationMotionContactDataType.ContactArcCenter

Contact arc center -------------------------------------

Field Value Type:NXOpen.Point3d

ContactArcRadius

CamOperationMotionContactDataType.ContactArcRadius

Contact arc radius -------------------------------------

Field Value Type:float

ContactShape

CamOperationMotionContactDataType.ContactShape

-------------------------------------

Field Value Type:NXOpen.CAM.CamOperationMotionShapeType