CamOperationMotionShapeType Enumeration

class NXOpen.CAM.CamOperationMotionShapeType

Bases: object

Motion shape types Enum Members

Enum Member Enum Member Description
Undefined
Linear
CircularCw
CircularCcw
Point
HelicalCw
HelicalCcw
Nurbs
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.