BoundaryTurnVariableStock Class¶
-
class
NXOpen.CAM.
BoundaryTurnVariableStock
¶ Bases:
NXOpen.TaggedObject
Represents a BoundaryTurnVariableStock
This is an abstract class and cannot be instantiated.
New in version NX9.0.2.
Properties¶
Property | Description |
---|---|
PositionalValues | Returns or sets the positional values |
StockList | Returns the stock list |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CreateItemBuilder | Create a new set |
Enumerations¶
BoundaryTurnVariableStockPositionType Enumeration | the position types available |
Property Detail¶
PositionalValues¶
-
BoundaryTurnVariableStock.
PositionalValues
¶ Returns or sets the positional values
-------------------------------------
Getter Method
Signature
PositionalValues
Returns: Return type: NXOpen.CAM.BoundaryTurnVariableStockPositionType
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
PositionalValues
Parameters: positionalValues ( NXOpen.CAM.BoundaryTurnVariableStockPositionType
) –New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
StockList¶
-
BoundaryTurnVariableStock.
StockList
¶ Returns the stock list
-------------------------------------
Getter Method
Signature
StockList
Returns: Return type: NXOpen.CAM.BoundaryTurnVariableStockSetList
New in version NX9.0.2.
License requirements: None.
Method Detail¶
CreateItemBuilder¶
-
BoundaryTurnVariableStock.
CreateItemBuilder
¶ Create a new set
Signature
CreateItemBuilder()
Returns: the variable stock set object Return type: NXOpen.CAM.BoundaryTurnVariableStockSet
New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)