BoundaryTurnVariableStockPositionType Enumeration

NXOpen.CAM.BoundaryTurnVariableStock.PositionType is an alias for NXOpen.CAM.BoundaryTurnVariableStockPositionType

class NXOpen.CAM.BoundaryTurnVariableStockPositionType

Bases: object

the position types available

Enum Members

Enum Member Enum Member Description
Distance
Percent
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.