BoundarySetPlanarMill Class¶
-
class
NXOpen.CAM.
BoundarySetPlanarMill
¶ Bases:
NXOpen.CAM.BoundarySet
Represents a boundary set for the planar mill/surface contour operation
To create a new instance of this class, use
NXOpen.CAM.Boundary.CreateBoundarySetPlanarMill()
New in version NX11.0.1.
Properties¶
Property | Description |
---|---|
BlankDistance | Returns or sets the blank_distance |
BoundaryMemberList | Returns the boundary member list |
BoundaryType | Returns or sets the boundary type |
CustomBlankDistance | Returns or sets the blank distance |
CustomFeed | Returns or sets the feed rate toggle |
CustomOffset | Returns or sets the flag whether this boundary has custom offset activated |
CustomStock | Returns or sets the flag whether this boundary has custom stock activated |
CustomTolerance | Returns or sets the tolerance toggle |
FeedUnit | Returns or sets the feed rate unit |
FeedValue | Returns or sets the feed rate value |
InTolerance | Returns or sets the in tolerance |
Offset | Returns or sets the offset value |
OffsetIntent | Returns or sets the offset intent |
OutTolerance | Returns or sets the out tolerance |
Plane | Returns or sets the boundary plane |
PlaneType | Returns or sets the boundary plane type |
PointList | Returns the points list |
SelectObject | Returns the select object |
Stock | Returns or sets the stock value |
Tag | Returns the Tag for this object. |
ToolPosition | Returns or sets the tool position |
ToolSide | Returns or sets the tool side |
Methods¶
Method | Description |
---|---|
AppendCurves | Add curves to the boundary |
CreateBoundaryMemberSet | Create an empty boundary member set |
CreateBoundaryMemberSetPlanarMill | Create an empty custom member data set for a planar mill/surface contour boundary |
CreateCurveBoundaryFromPermanent | Create curve boundary from permanent one |
ExtendOrTrimEndPoint | Trim or extend the end point of a closed boundary |
ExtendOrTrimStartPoint | Trim or extend the start point of an open boundary |
MoveStartPoint | Move the start point of a closed boundary |
RemoveCurves | Remove curves from the boundary |
Enumerations¶
BoundarySetPlanarMillFeedUnitTypes Enumeration | the types available for the feed rate unit |
BoundarySetPlanarMillTrimExtendPosition Enumeration | the boundary position where to trim or to extend |
Property Detail¶
BlankDistance¶
-
BoundarySetPlanarMill.
BlankDistance
¶ Returns or sets the blank_distance
-------------------------------------
Getter Method
Signature
BlankDistance
Returns: Return type: float New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
BlankDistance
Parameters: newValue (float) – New in version NX11.0.1.
License requirements: cam_base (“CAM BASE”)
CustomBlankDistance¶
-
BoundarySetPlanarMill.
CustomBlankDistance
¶ Returns or sets the blank distance
-------------------------------------
Getter Method
Signature
CustomBlankDistance
Returns: Return type: bool New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
CustomBlankDistance
Parameters: newValue (bool) – New in version NX11.0.1.
License requirements: cam_base (“CAM BASE”)
CustomFeed¶
-
BoundarySetPlanarMill.
CustomFeed
¶ Returns or sets the feed rate toggle
-------------------------------------
Getter Method
Signature
CustomFeed
Returns: Return type: bool New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
CustomFeed
Parameters: newValue (bool) – New in version NX11.0.1.
License requirements: cam_base (“CAM BASE”)
CustomStock¶
-
BoundarySetPlanarMill.
CustomStock
¶ Returns or sets the flag whether this boundary has custom stock activated
-------------------------------------
Getter Method
Signature
CustomStock
Returns: Return type: bool New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
CustomStock
Parameters: newValue (bool) – New in version NX11.0.1.
License requirements: cam_base (“CAM BASE”)
CustomTolerance¶
-
BoundarySetPlanarMill.
CustomTolerance
¶ Returns or sets the tolerance toggle
-------------------------------------
Getter Method
Signature
CustomTolerance
Returns: Return type: bool New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
CustomTolerance
Parameters: newValue (bool) – New in version NX11.0.1.
License requirements: cam_base (“CAM BASE”)
FeedUnit¶
-
BoundarySetPlanarMill.
FeedUnit
¶ Returns or sets the feed rate unit
-------------------------------------
Getter Method
Signature
FeedUnit
Returns: Return type: NXOpen.CAM.BoundarySetPlanarMillFeedUnitTypes
New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
FeedUnit
Parameters: newUnit ( NXOpen.CAM.BoundarySetPlanarMillFeedUnitTypes
) –New in version NX11.0.1.
License requirements: cam_base (“CAM BASE”)
FeedValue¶
-
BoundarySetPlanarMill.
FeedValue
¶ Returns or sets the feed rate value
-------------------------------------
Getter Method
Signature
FeedValue
Returns: Return type: float New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
FeedValue
Parameters: newValue (float) – New in version NX11.0.1.
License requirements: cam_base (“CAM BASE”)
InTolerance¶
-
BoundarySetPlanarMill.
InTolerance
¶ Returns or sets the in tolerance
-------------------------------------
Getter Method
Signature
InTolerance
Returns: Return type: float New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
InTolerance
Parameters: newValue (float) – New in version NX11.0.1.
License requirements: cam_base (“CAM BASE”)
OutTolerance¶
-
BoundarySetPlanarMill.
OutTolerance
¶ Returns or sets the out tolerance
-------------------------------------
Getter Method
Signature
OutTolerance
Returns: Return type: float New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
OutTolerance
Parameters: newValue (float) – New in version NX11.0.1.
License requirements: cam_base (“CAM BASE”)
Stock¶
-
BoundarySetPlanarMill.
Stock
¶ Returns or sets the stock value
-------------------------------------
Getter Method
Signature
Stock
Returns: Return type: float New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
Stock
Parameters: newValue (float) – New in version NX11.0.1.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
CreateBoundaryMemberSetPlanarMill¶
-
BoundarySetPlanarMill.
CreateBoundaryMemberSetPlanarMill
¶ Create an empty custom member data set for a planar mill/surface contour boundary
Signature
CreateBoundaryMemberSetPlanarMill()
Returns: Return type: NXOpen.CAM.BoundaryMemberSetPlanarMill
New in version NX11.0.1.
License requirements: cam_base (“CAM BASE”)
CreateCurveBoundaryFromPermanent¶
-
BoundarySetPlanarMill.
CreateCurveBoundaryFromPermanent
¶ Create curve boundary from permanent one
Signature
CreateCurveBoundaryFromPermanent()
New in version NX11.0.1.
License requirements: cam_base (“CAM BASE”)
ExtendOrTrimEndPoint¶
-
BoundarySetPlanarMill.
ExtendOrTrimEndPoint
¶ Trim or extend the end point of a closed boundary
Signature
ExtendOrTrimEndPoint(distance)
Parameters: distance (float) – New in version NX11.0.1.
License requirements: cam_base (“CAM BASE”)
ExtendOrTrimStartPoint¶
-
BoundarySetPlanarMill.
ExtendOrTrimStartPoint
¶ Trim or extend the start point of an open boundary
Signature
ExtendOrTrimStartPoint(distance)
Parameters: distance (float) – New in version NX11.0.1.
License requirements: cam_base (“CAM BASE”)
MoveStartPoint¶
-
BoundarySetPlanarMill.
MoveStartPoint
¶ Move the start point of a closed boundary
Signature
MoveStartPoint(bndSet, distance)
Parameters: - bndSet (
NXOpen.CAM.BoundaryMemberSetPlanarMill
) – - distance (float) –
New in version NX11.0.1.
License requirements: cam_base (“CAM BASE”)
- bndSet (