BoundarySetPlanarMillTrimExtendPosition Enumeration¶
NXOpen.CAM.BoundarySetPlanarMill.TrimExtendPosition is an alias for NXOpen.CAM.BoundarySetPlanarMillTrimExtendPosition
-
class
NXOpen.CAM.
BoundarySetPlanarMillTrimExtendPosition
¶ Bases:
object
the boundary position where to trim or to extend
Enum Members
Enum Member Enum Member Description AtStart trim or extend at start AtEnd trim or extend at end AtStartAndEnd trim or extend at start and at end Unknown unknown -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-