BladeFinish Class¶
-
class
NXOpen.CAM.
BladeFinish
¶ Bases:
NXOpen.CAM.Blade
Represents a Blade Finish Drive Method Builder
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
CutDirection | Returns or sets the Cut Direction |
CutPattern | Returns the cut pattern builder |
GeometryToFinish | Returns the Geometry to Finish |
LeadingEdge | Returns the leading edge builder |
SidesToCut | Returns the Sides to Cut |
StartPoint | Returns the Start Point |
Tag | Returns the Tag for this object. |
TrailingEdge | Returns the trailing edge builder |
Methods¶
Property Detail¶
GeometryToFinish¶
-
BladeFinish.
GeometryToFinish
¶ Returns the Geometry to Finish
-------------------------------------
Getter Method
Signature
GeometryToFinish
Returns: the Geometry to Finish Return type: NXOpen.CAM.BladeFinishGeom
New in version NX7.5.0.
License requirements: None.
SidesToCut¶
-
BladeFinish.
SidesToCut
¶ Returns the Sides to Cut
-------------------------------------
Getter Method
Signature
SidesToCut
Returns: the Sides to Cut Return type: NXOpen.CAM.CutSides
New in version NX7.5.0.
License requirements: None.
StartPoint¶
-
BladeFinish.
StartPoint
¶ Returns the Start Point
-------------------------------------
Getter Method
Signature
StartPoint
Returns: the Start Point Return type: NXOpen.CAM.BladeStartPoint
New in version NX7.5.0.
License requirements: None.