UnitSystem Enumeration¶
-
class
NXOpen.CAE.Xyplot.
UnitSystem
¶ Bases:
object
Represents the unit system
Deprecated since version NX12.0.0: Use
NXOpen.CAE.XyFunctionUnitSystem
Enum Members
Enum Member Enum Member Description Function Function unit Model Model unit Si International standard unit Mn Milliforce unit Mm Millimeter unit In Inch unit Custom Custom unit -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-