XyFunctionUnitSystem Enumeration¶
-
class
NXOpen.CAE.
XyFunctionUnitSystem
¶ Bases:
object
Represents the unit system Enum Members
Enum Member Enum Member Description Function Function unit Model Model unit MetricBase the Metric Base unit EnglishBase the English Base unit MetricCaeBase the Metric CAE Base EnglishCaeBase the English CAE Base Si International standard unit Custom Custom unit -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-