NoteStyleSetting Class¶
-
class
NXOpen.CAE.Xyplot.
NoteStyleSetting
¶ Bases:
NXOpen.CAE.Xyplot.TextStyleSetting
Represents the note display style.
Call
CAE.Xyplot.BaseDisplayStyleSetting.CommitChange()
to apply style changes to corresponding plot after it’s modified.Not support KF.
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
Alignment | Returns or sets the text alignment. |
Color | Returns or sets the text color |
Font | Returns or sets the text font |
FontStyle | Returns or sets the text font style. |
FontType | Returns or sets the text font type |
GlobalSizeScale | Returns or sets the scale of global text size. |
IsGlobalSizeAutoScaled | Returns or sets a value indicating whether to automatically adjust the scale of global text size to fit the screen. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
LeaderStyle | Returns the leader style |
NumberFormat | Returns the number format options |
Orientation | Returns or sets the text orientation. |
Owner | Returns the owner style |
Size | Returns or sets the text size. |
Tag | Returns the Tag for this object. |
TextBoxStyle | Returns the style of text box |
UseGlobalFontSetting | Returns or sets a value indicating whether to use the global setting of text font, font style and font size. |
Visibility | Returns or sets the visibility |
Weight | Returns or sets the text weight. |
Methods¶
Method | Description |
---|---|
CommitChange | Commits any edits that have been applied to the display style. |
Find | Finds the NXOpen.TaggedObject with the given identifier as recorded in a journal. |
GetNoteTexts | Gets the note texts |
SetNoteTexts | Sets the note texts |
Property Detail¶
Owner¶
-
NoteStyleSetting.
Owner
¶ Returns the owner style
-------------------------------------
Getter Method
Signature
Owner
Returns: Return type: NXOpen.CAE.Xyplot.IDisplayStyle
New in version NX10.0.0.
License requirements: None.
Visibility¶
-
NoteStyleSetting.
Visibility
¶ Returns or sets the visibility
-------------------------------------
Getter Method
Signature
Visibility
Returns: Return type: bool New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Visibility
Parameters: visibility (bool) – New in version NX12.0.0.
License requirements: None.
Method Detail¶
CommitChange¶
-
NoteStyleSetting.
CommitChange
¶ Commits any edits that have been applied to the display style.
Triggers the corresponding plot to update graph.
Signature
CommitChange()
New in version NX9.0.0.
License requirements: None.