BaseDisplayStyleSetting Class¶
-
class
NXOpen.CAE.Xyplot.
BaseDisplayStyleSetting
¶ Bases:
NXOpen.TaggedObject
,NXOpen.CAE.Xyplot.IDisplayStyle
Represent an abstract object on display style.
not support KF.
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Owner | Returns the owner style |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CommitChange | Commits any edits that have been applied to the display style. |
Find | Finds the NXOpen.TaggedObject with the given identifier as recorded in a journal. |
Property Detail¶
JournalIdentifier¶
-
BaseDisplayStyleSetting.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX12.0.0.
License requirements: None.
Owner¶
-
BaseDisplayStyleSetting.
Owner
¶ Returns the owner style
-------------------------------------
Getter Method
Signature
Owner
Returns: Return type: NXOpen.CAE.Xyplot.IDisplayStyle
New in version NX10.0.0.
License requirements: None.
Method Detail¶
CommitChange¶
-
BaseDisplayStyleSetting.
CommitChange
¶ Commits any edits that have been applied to the display style.
Triggers the corresponding plot to update graph.
Signature
CommitChange()
New in version NX9.0.0.
License requirements: None.
Find¶
-
BaseDisplayStyleSetting.
Find
¶ Finds the
NXOpen.TaggedObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
Find(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.TaggedObject
New in version NX12.0.0.
License requirements: None.