GeneralDisplayStyles Class¶
-
class
NXOpen.CAE.Xyplot.
GeneralDisplayStyles
¶ Bases:
NXOpen.CAE.Xyplot.BaseDisplayStyleSetting
Manages the general display styles.
Not support KF.
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Owner | Returns the owner style |
PhaseAngle | Returns or sets the phase angle in degree |
PhaseRangeOption | Returns or sets the phase range option |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CommitChange | Commits any edits that have been applied to the display style. |
Find | Finds the NXOpen.TaggedObject with the given identifier as recorded in a journal. |
Property Detail¶
Owner¶
-
GeneralDisplayStyles.
Owner
¶ Returns the owner style
-------------------------------------
Getter Method
Signature
Owner
Returns: Return type: NXOpen.CAE.Xyplot.IDisplayStyle
New in version NX10.0.0.
License requirements: None.
PhaseAngle¶
-
GeneralDisplayStyles.
PhaseAngle
¶ Returns or sets the phase angle in degree
-------------------------------------
Getter Method
Signature
PhaseAngle
Returns: Phase angle Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PhaseAngle
Parameters: phaseAngle (float) – Phase angle New in version NX10.0.0.
License requirements: None.
PhaseRangeOption¶
-
GeneralDisplayStyles.
PhaseRangeOption
¶ Returns or sets the phase range option
-------------------------------------
Getter Method
Signature
PhaseRangeOption
Returns: Phase range option Return type: NXOpen.CAE.Xyplot.PhaseRangeOption
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PhaseRangeOption
Parameters: phaseRangeOption ( NXOpen.CAE.Xyplot.PhaseRangeOption
) – Phase range optionNew in version NX10.0.0.
License requirements: None.