ColorScaleStyle Class¶
-
class
NXOpen.CAE.Xyplot.
ColorScaleStyle
¶ Bases:
NXOpen.CAE.Xyplot.BaseDisplayStyleSetting
Represents the color scale display style.
Call
CAE.Xyplot.BaseDisplayStyleSetting.CommitChange()
to apply style changes to corresponding plot after it’s modified.Not support KF.
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
AutoLevel | Returns or sets the option indicates whether to define color level automatically |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Level | Returns or sets the level setting |
Owner | Returns the owner style |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CommitChange | Commits any edits that have been applied to the display style. |
Find | Finds the NXOpen.TaggedObject with the given identifier as recorded in a journal. |
Property Detail¶
AutoLevel¶
-
ColorScaleStyle.
AutoLevel
¶ Returns or sets the option indicates whether to define color level automatically
-------------------------------------
Getter Method
Signature
AutoLevel
Returns: Auto level setting Return type: bool New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AutoLevel
Parameters: useAutoLevel (bool) – Auto Level setting New in version NX12.0.0.
License requirements: None.
Level¶
-
ColorScaleStyle.
Level
¶ Returns or sets the level setting
-------------------------------------
Getter Method
Signature
Level
Returns: level setting Return type: int New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Level
Parameters: level (int) – Level setting New in version NX11.0.0.
License requirements: None.
Owner¶
-
ColorScaleStyle.
Owner
¶ Returns the owner style
-------------------------------------
Getter Method
Signature
Owner
Returns: Return type: NXOpen.CAE.Xyplot.IDisplayStyle
New in version NX10.0.0.
License requirements: None.