ColorMapPlot Class¶
-
class
NXOpen.CAE.Xyplot.
ColorMapPlot
¶ Bases:
NXOpen.CAE.Xyplot.Plot
,NXOpen.CAE.Xyplot.I3DDataPlot
Manages the display of color map plot.
Call
CAE.Xyplot.I3DDataPlot.EditRecords()
to edit data for this class.Not support KF.
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
PlotTemplate | Returns the plot template |
Prototype | Returns the prototype of this object if it is an occurrence. |
SubGraphCountInStack | Returns the sub-graph count in a stacked plot. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CommitRecordsChange | Accepts record changed and process data to update data model |
CreateAttributeIterator | Create an attribute iterator |
CreateNote | Creates a note on the plot |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteRecord | Deletes the nth record. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
EditRecords | Edits records of plot. |
Find | Finds the NXObject with the given identifier as recorded in a journal. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
FitAxisLimit | Update axis limits for an overlaying plot if current displayed axis limits in plot do not fit for all records. |
FitView | Fits the display view on a reasonable region. |
GetApplicationDataOfRecord | Returns application specific data associated to a record. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetDeviceAndViewIndex | Gets the window device and view index of the plot graph. |
GetGraphs | Gets all graphs on the plot. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetLegendTables | Gets the legend table models on the plot. |
GetModels | Gets the models by model type. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetNotes | Gets all notes on the plot |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetRecordCount | Returns the count of plotted records on the plot graph. |
GetRecordDisplayVisibility | Gets the visibility of specified record. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetTitles | Gets the titles on the plot. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
GetViewBoundingBox | Gets the bounding box of the plot view. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
Prints a representation of this object to the system log file. | |
SaveRecords | Saves plotted records on a graph to an afu file. |
SaveRecordsToCsv | Saves plotted records on a plot graph to a CSV file. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetRecordDisplayVisibility | Sets the visibility of specified record. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
UpdateDisplay | Updates model display |
WriteToTemplateFile | Writes the template setting of plot to template file. |
Property Detail¶
IsOccurrence¶
-
ColorMapPlot.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
ColorMapPlot.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
ColorMapPlot.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
ColorMapPlot.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
ColorMapPlot.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
ColorMapPlot.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
EditRecords¶
-
ColorMapPlot.
EditRecords
¶ Edits records of plot.
** Procedure of editing records of plot fully:</b>
- Call this method to edit record data
- Call
CAE.Xyplot.Plot.CommitRecordsChange()
to precess record data change and update data model - Call
CAE.Xyplot.IDisplayableModel.UpdateDisplay()
to regenerate display to reflect data change - Optionally call
CAE.Xyplot.Plot.FitView()
to make display fit the view;it is only required when the plot display boundary is changed
Signature
EditRecords(records)
Parameters: records (list of NXOpen.CAE.FTK.BaseRecord
) –New in version NX12.0.0.
License requirements: None.
FindObject¶
-
ColorMapPlot.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Print¶
-
ColorMapPlot.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
ColorMapPlot.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.