BaseTemplateManager Class¶
-
class
NXOpen.CAE.Xyplot.
BaseTemplateManager
¶ Bases:
NXOpen.NXObject
Manages the graph template
Not support KF.
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
ActiveTemplate | Returns or sets the active template file |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CreateAttributeIterator | Create an attribute iterator |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteTemplate | Deletes template file |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetDefaultTemplate | Returns the default template file |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
LoadTemplate | Loads the graph template file |
Prints a representation of this object to the system log file. | |
ReloadAllTemplateFiles | Reload all graph template files so that the modification on the loaded graph template files are reset. |
RenameTemplateFile | Renames template file |
ResetSystemTemplate | Resets system template |
ResetTemplate | Resets to default value |
SaveAllTemplates | Saves all templates |
SaveAsTemplate | Saves to new template file |
SaveTemplate | Saves to template file |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetDefaultTemplate | Sets the default template file. |
SetName | Sets the custom name of the object. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
UnloadAllTemplates | Unloads all graph template files |
UnloadTemplate | Unloads the graph template file |
Property Detail¶
ActiveTemplate¶
-
BaseTemplateManager.
ActiveTemplate
¶ Returns or sets the active template file
-------------------------------------
Getter Method
Signature
ActiveTemplate
Returns: Template file name with full path Return type: str New in version NX7.5.0.
Deprecated since version NX12.0.0: Use
NXOpen.CAE.Xyplot.BaseTemplateManager.GetDefaultTemplate()
License requirements: None.
-------------------------------------
Setter Method
Signature
ActiveTemplate
Parameters: templateFile (str) – Template file name with full path New in version NX7.5.0.
Deprecated since version NX12.0.0: Use
NXOpen.CAE.Xyplot.BaseTemplateManager.SetDefaultTemplate()
License requirements: None.
IsOccurrence¶
-
BaseTemplateManager.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
BaseTemplateManager.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
BaseTemplateManager.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
BaseTemplateManager.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
BaseTemplateManager.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
BaseTemplateManager.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
DeleteTemplate¶
-
BaseTemplateManager.
DeleteTemplate
¶ Deletes template file
Signature
DeleteTemplate(templateFile)
Parameters: templateFile (str) – Template file name with full path New in version NX7.5.0.
License requirements: None.
FindObject¶
-
BaseTemplateManager.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetDefaultTemplate¶
-
BaseTemplateManager.
GetDefaultTemplate
¶ Returns the default template file
Signature
GetDefaultTemplate()
Returns: Template file name with full path Return type: str New in version NX12.0.0.
License requirements: None.
LoadTemplate¶
-
BaseTemplateManager.
LoadTemplate
¶ Loads the graph template file
Signature
LoadTemplate(templateFile)
Parameters: templateFile (str) – Template file name with full path New in version NX7.5.0.
License requirements: None.
Print¶
-
BaseTemplateManager.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
ReloadAllTemplateFiles¶
-
BaseTemplateManager.
ReloadAllTemplateFiles
¶ Reload all graph template files so that the modification on the loaded graph template files are reset.
The unloaded files under customer directories which is defined by environement variable UGII_BASE_DIR, UGII_VENDOR_DIR, UGII_SITE_DIR and UGII_USER_DIR will be reloaded. Also the graph templates in active root part directory will be reloaded if they are unloaded.
Signature
ReloadAllTemplateFiles()
New in version NX12.0.0.
License requirements: None.
RenameTemplateFile¶
-
BaseTemplateManager.
RenameTemplateFile
¶ Renames template file
Signature
RenameTemplateFile(oldTemplateFile, newTemplateFileName)
Parameters: - oldTemplateFile (str) – old template file with full path
- newTemplateFileName (str) – new template file with simple name.
New in version NX12.0.0.
License requirements: None.
ResetSystemTemplate¶
-
BaseTemplateManager.
ResetSystemTemplate
¶ Resets system template
Signature
ResetSystemTemplate()
New in version NX12.0.0.
License requirements: None.
ResetTemplate¶
-
BaseTemplateManager.
ResetTemplate
¶ Resets to default value
Signature
ResetTemplate(templateFile)
Parameters: templateFile (str) – Template file name with full path New in version NX7.5.0.
License requirements: None.
SaveAllTemplates¶
-
BaseTemplateManager.
SaveAllTemplates
¶ Saves all templates
Signature
SaveAllTemplates()
New in version NX12.0.0.
License requirements: None.
SaveAsTemplate¶
-
BaseTemplateManager.
SaveAsTemplate
¶ Saves to new template file
Signature
SaveAsTemplate(sourceTemplateFile, destinationTemplateFile)
Parameters: - sourceTemplateFile (str) – Source template file name with full path
- destinationTemplateFile (str) – Destination template file name with full path
New in version NX7.5.0.
License requirements: None.
SaveTemplate¶
-
BaseTemplateManager.
SaveTemplate
¶ Saves to template file
Signature
SaveTemplate(templateFile)
Parameters: templateFile (str) – Template file name with full path New in version NX7.5.0.
License requirements: None.
SetDefaultTemplate¶
-
BaseTemplateManager.
SetDefaultTemplate
¶ Sets the default template file.
If the input template file is NULL, it will remove default template state.
If the input template file is not NULL, it will set the input template as default template.
Signature
SetDefaultTemplate(templateFile)
Parameters: templateFile (str) – Template file name with full path New in version NX12.0.0.
License requirements: None.
SetName¶
-
BaseTemplateManager.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.