AxisYStyleSetting Class¶
-
class
NXOpen.CAE.Xyplot.
AxisYStyleSetting
¶ Bases:
NXOpen.CAE.Xyplot.AxisStyleSetting
Represents the axis y display style.
Call
CAE.Xyplot.BaseDisplayStyleSetting.CommitChange()
to apply style changes to corresponding plot after it’s modified.Not support KF.
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
AxisType | Returns or sets the axis scale type |
BarLowerLimit | Returns or sets the bar lower limit indicating whether a bar is plotted from minimum or zero position of axis y |
DbDecades | Returns or sets the number of dB decades to display. |
DbRef | Returns or sets the dB reference value for a dB axis type. |
DbScale | Returns or sets the dB scale. |
GraphOverhead | Returns or sets the round value to display. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
LimitsType | Returns or sets the limits type |
LogDecades | Returns or sets the number of Log decades to display. |
Owner | Returns the owner style |
Tag | Returns the Tag for this object. |
UnitSystem | Returns or sets the unit system |
UnitSystemType | Returns or sets the unit system type |
Methods¶
Method | Description |
---|---|
CommitChange | Commits any edits that have been applied to the display style. |
Find | Finds the NXOpen.TaggedObject with the given identifier as recorded in a journal. |
GetDBSettings | Gets the dB settings |
GetDisplayUnit | Gets display unit |
GetFixedLimits | Gets the fixed limits |
GetLabelStyle | Gets the label style |
GetNumberStyle | Gets the number style |
LogUnitChangedEvent | Logs an update event for changing display unit before committing AxisStyleSetting change. |
SetFixedLimits | Sets the fixed limits |
Property Detail¶
BarLowerLimit¶
-
AxisYStyleSetting.
BarLowerLimit
¶ Returns or sets the bar lower limit indicating whether a bar is plotted from minimum or zero position of axis y
-------------------------------------
Getter Method
Signature
BarLowerLimit
Returns: Bar Lower Limit Return type: bool New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BarLowerLimit
Parameters: barLowerLimit (bool) – Bar Lower Limit New in version NX12.0.0.
License requirements: None.
Owner¶
-
AxisYStyleSetting.
Owner
¶ Returns the owner style
-------------------------------------
Getter Method
Signature
Owner
Returns: Return type: NXOpen.CAE.Xyplot.IDisplayStyle
New in version NX10.0.0.
License requirements: None.