AngleAxisStyleSetting Class¶
-
class
NXOpen.CAE.Xyplot.
AngleAxisStyleSetting
¶ Bases:
NXOpen.CAE.Xyplot.BaseDisplayStyleSetting
,NXOpen.CAE.Xyplot.IVisibleDisplayStyle
Represents the angle axis display style.
Call
CAE.Xyplot.BaseDisplayStyleSetting.CommitChange()
to apply style changes to corresponding plot after it’s modified.Not support KF.
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
AngleUnit | Returns or sets the angle axis number unit |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
LineDisplaySettings | Returns the angle axis lines display styles |
Owner | Returns the owner style |
Tag | Returns the Tag for this object. |
Visibility | Returns or sets the visibility |
Methods¶
Method | Description |
---|---|
CommitChange | Commits any edits that have been applied to the display style. |
Find | Finds the NXOpen.TaggedObject with the given identifier as recorded in a journal. |
Property Detail¶
AngleUnit¶
-
AngleAxisStyleSetting.
AngleUnit
¶ Returns or sets the angle axis number unit
-------------------------------------
Getter Method
Signature
AngleUnit
Returns: Angle unit Return type: NXOpen.CAE.Xyplot.AngleUnit
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleUnit
Parameters: unit ( NXOpen.CAE.Xyplot.AngleUnit
) – Angle unitNew in version NX12.0.0.
License requirements: None.
LineDisplaySettings¶
-
AngleAxisStyleSetting.
LineDisplaySettings
¶ Returns the angle axis lines display styles
-------------------------------------
Getter Method
Signature
LineDisplaySettings
Returns: Angle axis lines display styles Return type: NXOpen.CAE.Xyplot.CurveDisplaySettings
New in version NX12.0.0.
License requirements: None.
Owner¶
-
AngleAxisStyleSetting.
Owner
¶ Returns the owner style
-------------------------------------
Getter Method
Signature
Owner
Returns: Return type: NXOpen.CAE.Xyplot.IDisplayStyle
New in version NX10.0.0.
License requirements: None.
Visibility¶
-
AngleAxisStyleSetting.
Visibility
¶ Returns or sets the visibility
-------------------------------------
Getter Method
Signature
Visibility
Returns: Return type: bool New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Visibility
Parameters: visibility (bool) – New in version NX12.0.0.
License requirements: None.