ViewLayoutManager Class¶
-
class
NXOpen.CAE.
ViewLayoutManager
¶ Bases:
object
Represents Interface to access CAE View Layout Manager object
To obtain an instance of this class, refer to
NXOpen.BasePart
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
Arrangement | Returns the cae view layout arrangement type |
Methods¶
Method | Description |
---|---|
SetArrangement | Sets the cae view layout arrangement type |
Enumerations¶
ViewLayoutManagerArrangementType Enumeration | Indicates the arrangement type of a layout. |
Property Detail¶
Arrangement¶
-
ViewLayoutManager.
Arrangement
¶ Returns the cae view layout arrangement type
-------------------------------------
Getter Method
Signature
Arrangement
Returns: Arrangement of layout Return type: NXOpen.CAE.ViewLayoutManagerArrangementType
New in version NX12.0.0.
License requirements: None.
Method Detail¶
SetArrangement¶
-
ViewLayoutManager.
SetArrangement
¶ Sets the cae view layout arrangement type
Signature
SetArrangement(arrangementType)
Parameters: arrangementType ( NXOpen.CAE.ViewLayoutManagerArrangementType
) – Arrangement of layoutNew in version NX12.0.0.
License requirements: None.