ViewLayoutManagerArrangementType Enumeration¶
NXOpen.CAE.ViewLayoutManager.ArrangementType is an alias for NXOpen.CAE.ViewLayoutManagerArrangementType
-
class
NXOpen.CAE.
ViewLayoutManagerArrangementType
¶ Bases:
object
Indicates the arrangement type of a layout.
New in version NX12.0.0.
Enum Members
Enum Member Enum Member Description Ly1 Ly2v Ly2h Ly4 Ly6v Ly9 Ly3 Ly3h Ly6h -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-