SphereBoundingVolume Class¶
-
class
NXOpen.CAE.
SphereBoundingVolume
¶ Bases:
NXOpen.CAE.BoundingVolumePrimitive
Represents Sphere Bounding Volume for Selection Recipe
This is a sub object
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
Containment | Returns or sets the contaiment for the Bounding Volume Primitive. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetCenterDiameter | Gets the center point and diameter for the Sphere Bounding Volume. |
GetCreationMethod | Gets the type for the Bounding Volume Primitive. |
SetCenterDiameter | Sets the center point and diameter for the Sphere Bounding Volume. |
Method Detail¶
GetCenterDiameter¶
-
SphereBoundingVolume.
GetCenterDiameter
¶ Gets the center point and diameter for the Sphere Bounding Volume.
Signature
GetCenterDiameter()
Returns: a tuple Return type: A tuple consisting of (centerPoint, diameter). centerPoint is a NXOpen.Point
. diameter is aNXOpen.Expression
.New in version NX12.0.0.
License requirements: None.
SetCenterDiameter¶
-
SphereBoundingVolume.
SetCenterDiameter
¶ Sets the center point and diameter for the Sphere Bounding Volume.
Signature
SetCenterDiameter(centerPoint, diameter)
Parameters: - centerPoint (
NXOpen.Point
) – - diameter (
NXOpen.Expression
) –
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- centerPoint (