BoundingVolumePrimitive Class¶
-
class
NXOpen.CAE.
BoundingVolumePrimitive
¶ Bases:
NXOpen.TaggedObject
Represents a Bounding Volume Primitive class
NXOpen.CAE.BoundingVolumePrimitive
.This is a sub object
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
Containment | Returns or sets the contaiment for the Bounding Volume Primitive. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetCreationMethod | Gets the type for the Bounding Volume Primitive. |
Property Detail¶
Containment¶
-
BoundingVolumePrimitive.
Containment
¶ Returns or sets the contaiment for the Bounding Volume Primitive.
-------------------------------------
Getter Method
Signature
Containment
Returns: Return type: NXOpen.CAE.CaeBoundingVolumePrimitiveContainment
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Containment
Parameters: containment ( NXOpen.CAE.CaeBoundingVolumePrimitiveContainment
) –New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Method Detail¶
GetCreationMethod¶
-
BoundingVolumePrimitive.
GetCreationMethod
¶ Gets the type for the Bounding Volume Primitive.
Signature
GetCreationMethod()
Returns: Return type: NXOpen.CAE.CaeBoundingVolumePrimitiveType
New in version NX12.0.0.
License requirements: None.