CaeBoundingVolumePrimitiveContainment Enumeration¶
-
class
NXOpen.CAE.
CaeBoundingVolumePrimitiveContainment
¶ Bases:
object
Used to specify the containment for the Bounding Volume Primitive. Enum Members
Enum Member Enum Member Description Inside completely inside the primitive InsideCrossing completely inside or partially inside the primitive -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-