SimSolutionStep Class¶
-
class
NXOpen.CAE.
SimSolutionStep
¶ Bases:
NXOpen.CAE.SimGroupContainer
Represents a subcase/step in a solution.
For more information, refer to the Solver language documentation in the SolverLanguageDocumentation.
To create a new instance of this class, use
NXOpen.CAE.SimSimulation.CreateSolutionStep()
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
IsConstraintGroupAllowed | Returns a value indicating whether a constraint group is allowed for this group container |
IsLoadGroupAllowed | Returns a value indicating whether a load group is allowed for this group container |
IsOccurrence | Returns whether this object is an occurrence or not. |
IsSimulationObjectGroupAllowed | Returns a value indicating whether a simulation object group is allowed for this group container |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
PropertyTable | Returns the property table associated with the step |
Prototype | Returns the prototype of this object if it is an occurrence. |
Solution | Returns the solution to which the step belongs |
StepType | Returns the step type |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AddBc | Add the bc to the step Only the BC that not under the folder can be added to solution |
AddFolder | Add the folder to the solution Only the folder not under other folder can be added to solution. |
CloneStep | Clone the solution step |
CreateAttributeIterator | Create an attribute iterator |
CreateConstraintGroup | Creates a constraint group for a solution or solution step |
CreateLoadGroup | Creates a load group for a solution or solution step |
CreateSimulationObjectGroup | Creates a simulation object group for a solution or solution step |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteGroup | Deletes a BC group from this group container |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
Find | Returns the children of the Solution Step of the given Identifier |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBcs | Gets all the BCs in this solution step |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetFolders | Gets all the root folders in this solution step |
GetGroupCount | Returns the number of groups in this container |
GetGroups | Gets the BC groups in this group container |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUnfolderedBcs | Gets all the unfoldered BCs in this solution |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
Prints a representation of this object to the system log file. | |
RemoveAllConstraints | Remove all constraints from the step |
RemoveAllLoads | Remove all loads from the step |
RemoveAllSimulationObjects | Remove all simulation objects from the step |
RemoveBc | Remove the bc from the step Only the BC that not under the folder can be removed from solution |
RemoveFolder | Remove the folder from the solution Only the folder not under other folder can be removed from solution. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Property Detail¶
IsOccurrence¶
-
SimSolutionStep.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
SimSolutionStep.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
SimSolutionStep.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
SimSolutionStep.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
SimSolutionStep.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
PropertyTable¶
-
SimSolutionStep.
PropertyTable
¶ Returns the property table associated with the step
-------------------------------------
Getter Method
Signature
PropertyTable
Returns: property table Return type: NXOpen.CAE.PropertyTable
New in version NX4.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Prototype¶
-
SimSolutionStep.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Solution¶
-
SimSolutionStep.
Solution
¶ Returns the solution to which the step belongs
-------------------------------------
Getter Method
Signature
Solution
Returns: the solution to which the step belongs Return type: NXOpen.CAE.SimSolution
New in version NX4.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Method Detail¶
AddBc¶
-
SimSolutionStep.
AddBc
¶ Add the bc to the step Only the BC that not under the folder can be added to solution
Signature
AddBc(bc)
Parameters: bc ( NXOpen.CAE.SimBC
) – the bc to be addedNew in version NX4.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
AddFolder¶
-
SimSolutionStep.
AddFolder
¶ Add the folder to the solution Only the folder not under other folder can be added to solution.
Signature
AddFolder(folder)
Parameters: folder ( NXOpen.CAE.SimLbcFolder
) – the folder to be addedNew in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CloneStep¶
-
SimSolutionStep.
CloneStep
¶ Clone the solution step
Signature
CloneStep(suggestedName)
Parameters: suggestedName (str) – name to use instead of default name (may be None) Returns: the newly created NXOpen.CAE.SimSolutionStep
Return type: NXOpen.CAE.SimSolutionStep
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Find¶
-
SimSolutionStep.
Find
¶ Returns the children of the Solution Step of the given Identifier
Signature
Find(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.TaggedObject
New in version NX10.0.0.
License requirements: None.
FindObject¶
-
SimSolutionStep.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetBcs¶
-
SimSolutionStep.
GetBcs
¶ Gets all the BCs in this solution step
Signature
GetBcs()
Returns: Resultant bcs Return type: list of NXOpen.CAE.SimBC
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetFolders¶
-
SimSolutionStep.
GetFolders
¶ Gets all the root folders in this solution step
Signature
GetFolders()
Returns: Resultant bcs Return type: list of NXOpen.CAE.SimLbcFolder
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetUnfolderedBcs¶
-
SimSolutionStep.
GetUnfolderedBcs
¶ Gets all the unfoldered BCs in this solution
Signature
GetUnfolderedBcs()
Returns: Resultant bcs Return type: list of NXOpen.CAE.SimBC
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Print¶
-
SimSolutionStep.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
RemoveAllConstraints¶
-
SimSolutionStep.
RemoveAllConstraints
¶ Remove all constraints from the step
Signature
RemoveAllConstraints()
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
RemoveAllLoads¶
-
SimSolutionStep.
RemoveAllLoads
¶ Remove all loads from the step
Signature
RemoveAllLoads()
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
RemoveAllSimulationObjects¶
-
SimSolutionStep.
RemoveAllSimulationObjects
¶ Remove all simulation objects from the step
Signature
RemoveAllSimulationObjects()
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
RemoveBc¶
-
SimSolutionStep.
RemoveBc
¶ Remove the bc from the step Only the BC that not under the folder can be removed from solution
Signature
RemoveBc(bc)
Parameters: bc ( NXOpen.CAE.SimBC
) – the bc to be removeNew in version NX4.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
RemoveFolder¶
-
SimSolutionStep.
RemoveFolder
¶ Remove the folder from the solution Only the folder not under other folder can be removed from solution.
Signature
RemoveFolder(folder)
Parameters: folder ( NXOpen.CAE.SimLbcFolder
) – the folder to be removedNew in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetName¶
-
SimSolutionStep.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.