SimPart Class¶
-
class
NXOpen.CAE.
SimPart
¶ Bases:
NXOpen.CAE.CaePart
Represents an NX part of type .sim.
Use the
NXOpen.PartCollection
class to load or create a part.New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
ComponentAssembly | Returns the component assembly. |
Displayed | Returns true if the part represents a displayed part. |
FemPart | Returns the fem part associated with the sim part |
FieldManager | Returns the field main. |
FullPath | Returns the full path of the part. |
HasWriteAccess | Returns the write-access status of a part independent of the load state. |
IsFullyLoaded | Returns the load status of a part. |
IsOccurrence | Returns whether this object is an occurrence or not. |
IsReadOnly | Returns the read-only status of a part. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Leaf | Returns the leaf name of the part. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
PartPreviewMode | Returns or sets the preview mode |
PartUnits | Returns the units of the part file. |
Prototype | Returns the prototype of this object if it is an occurrence. |
SaveDisplayFacets | Returns or sets whether display quality facets are saved in the part file |
Simulation | Returns the NXOpen.CAE.SimSimulation object |
Tag | Returns the Tag for this object. |
UniqueIdentifier | Returns or sets the unique identifier for this part used to determine whether parts can be quietly substituted during part open. |
Methods¶
Method | Description |
---|---|
AssignPermanentName | Saves a temporary part with the given name. |
CanBeDisplayPart | Returns true if the part can be displayed and false if not displayed. |
Close | Closes an open part. |
CompleteStructure | Make additions necessary to complete the incomplete assembly structure of the input part |
CompressLabels | Compress the labels of csys, physical, and groups |
CreateAttributeIterator | Create an attribute iterator |
CreateConvertToConvergentBodyBuilder | Creates a NXOpen.CAE.ConvertToConvergentBodyBuilder |
CreateDynamicSectionBuilder | Creates a NXOpen.Display.DynamicSectionBuilder The base part must be a displayable part, otherwise an exception will be thrown. |
CreateEffectivityConditionBuilder | Creates a NXOpen.EffectivityConditionBuilder |
CreateFacetSettingsBuilder | Creates a builder for the Facet Settings dialog |
CreateGatewayGroupBuilder | Creates a Groups builder |
CreateImportSimBuilder | Creates ImportSimulationBuilder. |
CreateModelDisplayBuilder | Creates a builder for model display controls command |
CreatePerspectiveOptionsBuilder | Creates a builder for the Perspective Options dialog |
CreateReferenceSet | Creates a NXOpen.ReferenceSet object |
CreateSolverAppendOption | Returns a solver append option object for importing the solver specific data into an existing NXOpen.CAE.FemPart or NXOpen.CAE.SimPart . |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteReferenceSet | Deletes a NXOpen.ReferenceSet object |
DeleteSolverAppendOption | Deletes a solver append option object for importing the solver specific data into an existing NXOpen.CAE.FemPart or NXOpen.CAE.SimPart . |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
ExportJt | Exports JT file |
ExportSimulation | Exports the Simulation data for a NXOpen.CAE.CaePart . |
FinalizeCreation | Finalizes the creation of the sim part file. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAllReferenceSets | Get all the NXOpen.ReferenceSet objects in this part. |
GetApplication | Get the application which corresponds to the specified type. |
GetArrangements | Outputs the NXOpen.Assemblies.Arrangement objects within the given part. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetCollaborativeContentType | The collaborative content type of this part. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetCsysFlattenedLabel | Gets the resolved label of csys in cae part. |
GetDescription | Gets the description assoicated with the Cae part |
GetHistoryInformation | Get history of part |
GetIncompleteStatus | Inquire whether the provided part is flagged as being incomplete |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetMakeUniqueName | Gets the Unique name on a part for the Make Unique operation |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetPreviewImage | Get the preview image This will return the graphic preview image of the part (when available). |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetTransientStatus | Inquire whether the provided part is flagged as being transient |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
ImportExistingSimulation | Imports the solver specific data into an existing NXOpen.CAE.FemPart or NXOpen.CAE.SimPart . |
ImportSim | Imports all entities of selected type from the source sim into the current (target) sim. |
LoadFeatureDataForSelection | Ensure that feature data is loaded for a part. |
LoadFully | Ensures that this part is fully loaded. |
LoadThisPartFully | Ensures that this part is fully loaded. |
LoadThisPartPartially | Ensures that this part is at least partially loaded. |
NewBeamSectionOffsetOptions | Creates a NXOpen.CAE.BeamSectionOffsetOptions |
NewBeamSectionOptions | Creates a NXOpen.CAE.BeamSectionOptions |
NewBeamSectionOrientationOptions | Creates a NXOpen.CAE.BeamSectionOrientationOptions |
NewMaterialOptions | Creates a NXOpen.CAE.MaterialOptions |
Prints a representation of this object to the system log file. | |
RegenerateDisplayFacets | Regenerates display specific transient cached facets in the part. |
ReinstateTransience | Reinstate the transient status to the formerly transient input part |
RelabelByOffsets | Relabels the csys, physical, and group labels by the specified offset value |
RemoveTransience | Remove the transient status from the input part |
Reopen | Reopens a loaded part. |
ReopenAs | Reopens a loaded part. |
ReverseBlankAll | Reverse blank all the objects in the part. |
Save | Saves the part whether it is modified or not. |
SaveAs | Creates copy of target part. |
SaveBookmark | Saves a bookmark file. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetDescription | Sets the description assoicated with the Cae part |
SetMakeUniqueName | Sets the unique name on part for the Make Unique operation |
SetName | Sets the custom name of the object. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Undisplay | Undisplays the part, if it is currently a displayed part. |
Structs¶
SimPartImportErrorCodes_Struct Struct | Contains list of error codes for import of each entity type |
SimPartImportOptions_Struct Struct | Contains information about which entities to be imported |
Property Detail¶
FemPart¶
-
SimPart.
FemPart
¶ Returns the fem part associated with the sim part
-------------------------------------
Getter Method
Signature
FemPart
Returns: Fem part associated to the sim part Return type: NXOpen.CAE.CaePart
New in version NX4.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
IsOccurrence¶
-
SimPart.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
SimPart.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
SimPart.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
SimPart.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
SimPart.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
SimPart.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Simulation¶
-
SimPart.
Simulation
¶ Returns the
NXOpen.CAE.SimSimulation
object-------------------------------------
Getter Method
Signature
Simulation
Returns: NXOpen.CAE.SimSimulation
Return type: NXOpen.CAE.SimSimulation
New in version NX4.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Method Detail¶
CompressLabels¶
-
SimPart.
CompressLabels
¶ Compress the labels of csys, physical, and groups
Signature
CompressLabels(compressCsysLabels, compressPhysLabels, compressGroupLabels)
Parameters: - compressCsysLabels (bool) – compress the csys labels
- compressPhysLabels (bool) – compress the physical labels
- compressGroupLabels (bool) – compress the group labels
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateImportSimBuilder¶
-
SimPart.
CreateImportSimBuilder
¶ Creates ImportSimulationBuilder.
This imports selected entities of different type from the source sim into the current (target) sim.
Signature
CreateImportSimBuilder()
Returns: The ImportSimulationBuilder object Return type: NXOpen.CAE.ImportSimulationBuilder
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
FinalizeCreation¶
-
SimPart.
FinalizeCreation
¶ Overloaded method FinalizeCreation
FinalizeCreation(femPart, description)
FinalizeCreation(femPart, femLayerOpt, description)
-------------------------------------
Finalizes the creation of the sim part file. This method should be called immediately after creating the sim part file. This method should be called only once for each sim part file. The second call to the method will raise an error.
Signature
FinalizeCreation(femPart, description)
Parameters: - femPart (
NXOpen.CAE.CaePart
) – the fem part fileNXOpen.CAE.FemPart
- description (list of str) – description
New in version NX4.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Finalizes the creation of the sim part file. This method should be called immediately after creating the sim part file. This method should be called only once for each sim part file. The second call to the method will raise an error.
Signature
FinalizeCreation(femPart, femLayerOpt, description)
Parameters: - femPart (
NXOpen.CAE.CaePart
) – the fem part fileNXOpen.CAE.FemPart
- femLayerOpt (int) – layer option. -1 = USE_ORIGINAL, 0 = USE_WORK
- description (list of str) – description
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
FindObject¶
-
SimPart.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
ImportSim¶
-
SimPart.
ImportSim
¶ Imports all entities of selected type from the source sim into the current (target) sim.
The FeModelOccurrence of the target sim onto which the user needs to import needs to be passed in. The input will be an array of FeModelOccurrences, if user wants to import the same source sim onto multiple FeModelOccurrences of the target sim.
Signature
ImportSim(fileName, prependString, selOptions, selectedFemoccs)
Parameters: - fileName (str) – name of the source simulation file
- prependString (str) – string to prepend imported simulation entity names, can be NULL or empty
- selOptions (
NXOpen.CAE.SimPartImportOptions_Struct
) – options indicating the types of entities to be imported - selectedFemoccs (list of
NXOpen.CAE.FEModelOccurrence
) – Array of FeModelOccurrences to import ontoNXOpen.CAE.FEModelOccurrence
Returns: list of generated error codes during import
Return type: New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Print¶
-
SimPart.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
RelabelByOffsets¶
-
SimPart.
RelabelByOffsets
¶ Relabels the csys, physical, and group labels by the specified offset value
Signature
RelabelByOffsets(csysOffset, physOffset, groupOffset)
Parameters: - csysOffset (int) – csys offset
- physOffset (int) – physical offset
- groupOffset (int) – group offset
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SetName¶
-
SimPart.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.