SimLoadRecipeSourceCollection Class¶
-
class
NXOpen.CAE.
SimLoadRecipeSourceCollection
¶ Bases:
object
This class is a collection of
NXOpen.CAE.SimLoadRecipeSource
.To obtain an instance of this class, refer to
NXOpen.CAE.SimLoadRecipe
New in version NX10.0.0.
Methods¶
Method | Description |
---|---|
Create | Creates and adds a new NXOpen.CAE.SimLoadRecipeSource to the Load Recipe |
Delete | Delete a list of sources |
Find | Finds a Source with a specified path. |
Method Detail¶
Create¶
-
SimLoadRecipeSourceCollection.
Create
¶ Creates and adds a new
NXOpen.CAE.SimLoadRecipeSource
to the Load RecipeSignature
Create(path, readerType, formatType)
Parameters: - path (str) –
- readerType (str) –
- formatType (str) –
Returns: Return type: New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Delete¶
-
SimLoadRecipeSourceCollection.
Delete
¶ Delete a list of sources
Signature
Delete(sources)
Parameters: sources (list of NXOpen.CAE.SimLoadRecipeSource
) – The sources to be deletedNew in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Find¶
-
SimLoadRecipeSourceCollection.
Find
¶ Finds a Source with a specified path.
Signature
Find(path)
Parameters: path (str) – path to the source Returns: Return type: NXOpen.CAE.SimLoadRecipeSource
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)