SimLoadRecipeSource Class¶
-
class
NXOpen.CAE.
SimLoadRecipeSource
¶ Bases:
NXOpen.TaggedObject
This is the class handling the attributes of a source used by a load recipe.
Use CAE.SimLoadRecipeSourceCollection.Create
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
DefaultFunctionAttributes | Returns the default attributes (NXOpen.CAE.SimLoadRecipeFunctionAttributes ) of a NXOpen.CAE.SimLoadRecipeSource which are used to indicate the attributes of the functions in the data source. |
FormatType | Returns or sets the format type of a NXOpen.CAE.SimLoadRecipeSource . |
Path | Returns or sets the path of a NXOpen.CAE.SimLoadRecipeSource . |
ReaderType | Returns or sets the reader type of a NXOpen.CAE.SimLoadRecipeSource . |
SourceLabel | Returns or sets the label of a NXOpen.CAE.SimLoadRecipeSource . |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetPropertyTable | Get the NXOpen.BasePropertyTable of a NXOpen.CAE.SimLoadRecipeSource . |
Property Detail¶
DefaultFunctionAttributes¶
-
SimLoadRecipeSource.
DefaultFunctionAttributes
¶ Returns the default attributes (
NXOpen.CAE.SimLoadRecipeFunctionAttributes
) of aNXOpen.CAE.SimLoadRecipeSource
which are used to indicate the attributes of the functions in the data source.This might return null, which means that the format handler takes care of managing those attributes on its own (this is the case for Test.Lab files).
-------------------------------------
Getter Method
Signature
DefaultFunctionAttributes
Returns: Return type: NXOpen.CAE.SimLoadRecipeFunctionAttributes
New in version NX12.0.0.
License requirements: None.
FormatType¶
-
SimLoadRecipeSource.
FormatType
¶ Returns or sets the format type of a
NXOpen.CAE.SimLoadRecipeSource
.The available format types are declared in datasourcehandlers.xml file located in <NX_install_dir>/UGSTRUCTURES/cae_language directory.
This string correlates to the Name attribute of the FormatHandler elements.
-------------------------------------
Getter Method
Signature
FormatType
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FormatType
Parameters: formatType (str) – New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Path¶
-
SimLoadRecipeSource.
Path
¶ Returns or sets the path of a
NXOpen.CAE.SimLoadRecipeSource
.-------------------------------------
Getter Method
Signature
Path
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Path
Parameters: path (str) – New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ReaderType¶
-
SimLoadRecipeSource.
ReaderType
¶ Returns or sets the reader type of a
NXOpen.CAE.SimLoadRecipeSource
.The available reader types are declared in datasourcehandlers.xml file located in <NX_install_dir>/UGSTRUCTURES/cae_language directory.
This string correlates to the Type attribute of the FileFormat elements.
-------------------------------------
Getter Method
Signature
ReaderType
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReaderType
Parameters: readerType (str) – New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SourceLabel¶
-
SimLoadRecipeSource.
SourceLabel
¶ Returns or sets the label of a
NXOpen.CAE.SimLoadRecipeSource
.-------------------------------------
Getter Method
Signature
SourceLabel
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SourceLabel
Parameters: sourceLabel (str) – New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
GetPropertyTable¶
-
SimLoadRecipeSource.
GetPropertyTable
¶ Get the
NXOpen.BasePropertyTable
of aNXOpen.CAE.SimLoadRecipeSource
.NOTE: After changing the properties in the table,
Update.DoUpdate()
should be called.Signature
GetPropertyTable()
Returns: Return type: NXOpen.BasePropertyTable
New in version NX10.0.0.
License requirements: None.